Hi ,
We add chromium browser in the BSP 6.1.55_2.2.0 and test github website. The Chromium browser will be shutting down . We tested on i.MX8M Plus Evaluate Board. Can anyone help?
Hi , Thanks for your reply. We follow the i.MX Yocto Project User Guide Rev LF6.1.55_2.2.0 document to build the bsp.
The instructions are as follows :
$ mkdir imx-yocto-bsp
$ cd imx-yocto-bsp
$ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-mickledore -m imx-6.1.55-2.2.0.xml
$ repo sync
$ DISTRO=fsl-imx-wayland MACHINE=imx8mpevk source imx-setup-release.sh -b build-wayland
Add Chromium Browser on Wayland
Add this CORE_IMAGE_EXTRA_INSTALL += "chromium-ozone-wayland" in imx8mpevk.conf.
The path is at " /meta-imx/meta-bsp/conf/machine"
$ bitbake imx-image-full
When the bsp image is installed on the 8MP EVK board, you can follow the instructions to launch the chromium browser.
$ chromium --no-sandbox
Hi @hankwang
Gor reply from R&D as below.
For customer's case, users may need to add "--disable-gpu" to the command.
show as following:
"chromium --no-sandbox --disable-gpu "
Disables GPU hardware acceleration. If software renderer is not in place, then the GPU process won't launch. You can reference the following ling about Chromium's issue and usage:
1.Headless: make --disable-gpu flag unnecessary - chromium
2.Chromium - ArchWiki (archlinux.org)
3. List of Chromium Command Line Switches « Peter Beverloo
Regards
Harvey