Getting undefined exception on enabling Neon and VFP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Getting undefined exception on enabling Neon and VFP

Jump to solution
1,263 Views
harshitsingh
Contributor I

Hi,

I am trying to enable a neon and vfp for iMX6 quad Sabre lite board.

Initially when I was setting the target cpu as ‘Cortex-A9.no_neon.no_vfp’, then the code was working fine.

But not when I use the target cpu as ‘Cortex-A9’ only and enabling the VFP and neon using the code mentioned below:

MRC p15,0,r0,c1,c0,2 ; Read CPACR into r0

       ORR r0,r0,#(3<<20) ; OR in User and Privileged access for CP10

       ORR r0,r0,#(3<<22) ; OR in User and Privileged access for CP11

       BIC r0, r0, #(3<<30) ; Clear ASEDIS/D32DIS if set

       MCR p15,0,r0,c1,c0,2 ; Store new access permissions into CPACR

       ISB ; Ensure side-effect of CPACR is visible

       MOV r0,#(1<<30) ; Create value with FPEXC (bit 30) set in r0

       VMSR FPEXC,r0 ; Enable VFP and SIMD extensions

I get an undefined exception when I do a single stepping for the last instruction ‘VMSR FPEXC, r0’;

So could you please let me know what else need to be taken care of to get rid of this exception with Neon and VFP enabled.

Kindly let me know your feedback regarding this.

Thanks,

Harshit

Labels (1)
0 Kudos
Reply
1 Solution
774 Views
Yuri
NXP Employee
NXP Employee

Please use

mcr     p10,#0x7,r0,c8,c0,#0  /* msr     FPEXC,r0 in ARM assembly */

instead of

  VMSR FPEXC,r0

View solution in original post

0 Kudos
Reply
1 Reply
775 Views
Yuri
NXP Employee
NXP Employee

Please use

mcr     p10,#0x7,r0,c8,c0,#0  /* msr     FPEXC,r0 in ARM assembly */

instead of

  VMSR FPEXC,r0

0 Kudos
Reply