Hi, 
I have an enable pin connected to a peripheral that I want to maintain HIGH during normal mode and suspend mode ($systemctl suspend).
In the DTS:
IMX8QM_LVDS0_GPIO01_LSIO_GPIO1_IO05 0x00000061
Do you know how can I configure this pin to maintain its value when is in suspended mode?
Best regards.
 riteshmpatel
		
			riteshmpatel
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi @oscarabril,
I hope you are doing well.
Since the value of the register remains the same in the normal mode and suspend mode, no configurations are needed to be done.
Thanks & Regards,
Ritesh M Patel
Thanks, and if the register is different in suspend mode? How can I handle this?
Best regards.
Found one example in linux-imx\arch\arm64\boot\dts\freescale\imx8qm-mek.dts
And it matches the description in RM and scfw documents.
And LATCH should work, you can try it.
i.MX8QM has several settings in low power mode.
 riteshmpatel
		
			riteshmpatel
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi @oscarabril,
The register value remains the same in normal and suspend modes.
Thanks & Regards,
Ritesh M Patel