Fow what value i can set as following TBD, in MX8M_LPDDR4_RPA_v24.xlsx file ,when I want set 1866MHZ,thanks and best regards

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fow what value i can set as following TBD, in MX8M_LPDDR4_RPA_v24.xlsx file ,when I want set 1866MHZ,thanks and best regards

998 Views
jw216
Contributor I

Fow what value i can set as following TBD, in MX8M_LPDDR4_RPA_v24.xlsx file ,when I want set 1866MHZ,thanks and best regards

memory set0x3036006832TBD#HW_DRAM_PLL_CFG2_ADDR: For 1866MHz DDR speed, Configure DRAM PLL for 933MHz operation
0 Kudos
Reply
1 Reply

932 Views
igorpadykov
NXP Employee
NXP Employee

Hi charles

in general "TBD" values can be left in default state.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply