Flexcan in IMX8QM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Flexcan in IMX8QM

跳至解决方案
1,709 次查看
vinothkumars
Senior Contributor IV

Hi All,

 

In IMX8QM-MEK have Base Board and GPIO-EXPANDER is there for CAN.

But, In IMX8QM custom board we don't have Base board as well as GPIO EXPANDAR, So, I removed theses gpio expander in rear_view_camera but Flex-CAN still not working.

Will you please give me some advice which area do I needs to configure.

 

Regards,
Vinothkumar Sekar
0 项奖励
1 解答
1,694 次查看
vinothkumars
Senior Contributor IV

Thank you @igorpadykov for the quick reply.

 

I am using SDK 2.5.1 from this SDK CAN used the io expander. But, my custom board don't have the io expander (BOARD_ConfigureExpansionIO) and I removed it from the flexcan driver. But, still flexcan is not working.

Please find the driver file used in sdk.

 

Regards,
Vinothkumar Sekar

在原帖中查看解决方案

0 项奖励
2 回复数
1,700 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vinothkumar

 

one can look at M4 flexcan examples in M4 SDK_MEK-MIMX8QM available on

https://mcuxpresso.nxp.com/en/welcome

 

Best regards
igor

0 项奖励
1,695 次查看
vinothkumars
Senior Contributor IV

Thank you @igorpadykov for the quick reply.

 

I am using SDK 2.5.1 from this SDK CAN used the io expander. But, my custom board don't have the io expander (BOARD_ConfigureExpansionIO) and I removed it from the flexcan driver. But, still flexcan is not working.

Please find the driver file used in sdk.

 

Regards,
Vinothkumar Sekar
0 项奖励