Failed when forward life cycle to OEM close

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Failed when forward life cycle to OEM close

跳至解决方案
2,366 次查看
dlliweihua
Contributor III

Hello NXP experts,

I tried to forward my i.MX8DXP SoC lifecycle with sc_seco_forward_lifecycle( ) call,the lifecycle is one of the followin value:  

/** 
* SECO_LIFECYCLE_DEFAULT = (1U << 0) Default fab mode (early_fuses_pgrm not blown)
* SECO_LIFECYCLE_FAB = (1U << 1) Fab mode
* SECO_LIFECYCLE_NO_SECRETS = (1U << 2) No secrets
* SECO_LIFECYCLE_SECRETS = (1U << 3) With Secrets
* SECO_LIFECYCLE_SC_FW_CLSD = (1U << 4) SCU FW Closed
* SECO_LIFECYCLE_SECO_FW_CLSD = (1U << 5) SECO FW Closed
* SECO_LIFECYCLE_CLOSED = (1U << 6) Closed
* SECO_LIFECYCLE_CLOSED_FW = (1U << 7) Closed with FW
* SECO_LIFECYCLE_PART_RTN = (1U << Partial field return
* SECO_LIFECYCLE_RTN = (1U << 9) Field return
* SECO_LIFECYCLE_NO_RTN = (1U << 10) No Return

*/

But the "sc_seco_forward_lifecycle( )" function returns sucessfully only when lifecycle is  "SECO_LIFECYCLE_CLOSED_FW",any other value possible will result failure.

1. I have burned OEM SRK hash into fuse[730-745]

2. I used a boot image signed with the corresponding SGK

3. I called sc_seco_forward_lifecycle(ipcHndl, 16) , but it returned with error code 11.

The commands I used to sign the boot image are:

./cst -i csf_boot_image.txt -o ipl-imx8qxp-cpu_c0.imx.signed

./cst -i csf_fs_image.txt -o ifs-imx8qxp-cpu-graphics.imx.signed

The csf files are attached.

Please help to check what is lost or fault, thank you.

Best Regards.

Liweihua 

0 项奖励
1 解答
2,166 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

这个是正常的,刚刚烧录好的key,不能马上被使用,所以seco内部认为是没有key的,不能切换到oem closed,只有重启之后,key才会被seco读进去,然后才能切换到oem close

This is normal. The key that has just been burned cannot be used immediately, so seco internally thinks that there is no key and cannot be switched to oem closed. Only after restarting, the key will be read by seco, and then can be switched to oem close .

 

在原帖中查看解决方案

8 回复数
2,167 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

这个是正常的,刚刚烧录好的key,不能马上被使用,所以seco内部认为是没有key的,不能切换到oem closed,只有重启之后,key才会被seco读进去,然后才能切换到oem close

This is normal. The key that has just been burned cannot be used immediately, so seco internally thinks that there is no key and cannot be switched to oem closed. Only after restarting, the key will be read by seco, and then can be switched to oem close .

 

1,862 次查看
olivergraute
Contributor III

This Seco behavior is causing some headache during or production procedure. Because we need a extra reboot after fusing the keys to perform the ahab_close(). Unfortunately we need here a  "real reboot" and not a simple partition reset. To ensure that Seco is restarted we implemented a reset  by calling "sc_pm_reset" from U-Boot side. Then we can use sucessfully ahab_close on next boot but only if the U-Boot is also signed by the PKI  

0 项奖励
2,150 次查看
dlliweihua
Contributor III

Thanks a lot.

Liweihua

标记 (1)
0 项奖励
2,263 次查看
dlliweihua
Contributor III

Hello?

Can someone help with this problem?

Now the OEM close is successful,

but after burning the SRK Hash,

it need to restart target board one time.

Is there any way to update lifecycle successfully without restarting after burning SRK Hash?

I have searched the uboot codes, but not found any hint about this problem.

Thanks.

Liweihua

Thanks!

Liweihua

0 项奖励
2,353 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Liweihua 

 

one can look at suggestions provided on

https://community.nxp.com/t5/i-MX-Processors/About-the-SoC-lifecycle/m-p/1204107#M166948

 

Best regards
igor

0 项奖励
2,351 次查看
dlliweihua
Contributor III

Hello igorpadykov ,

The two suggestions provided on

https://community.nxp.com/t5/i-MX-Processors/About-the-SoC-lifecycle/m-p/1204107#M166948,

The method that use JTAG should be excluded firstly, because the environment we are facing is mass production site;

The second suggestion is what I want to ask, why it failed when I call sc_seco_forward_lifecycle(ipcHndl, 16)?

Are there any prerequisites for successful execution of this call with the second parameter equals 16?

Thank you.

Liweihua 

0 项奖励
2,344 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Liweihua 

 

for sc_seco_forward_lifecycle call usage one can look at SCFW (sc_fw_api_qx_b0.pdf)

documentation included in SCFW Porting Kit​

 

Best regards
igor

0 项奖励
2,331 次查看
dlliweihua
Contributor III

@igorpadykov

Now the OEM close is successful,

but after burning the SRK Hash,

it need to restart target board one time.

Is there any way to update lifecycle successfully without restarting after burning SRK Hash?

I have searched the uboot codes, but not found any hint about this problem.

Thanks.

Liweihua

标记 (1)
0 项奖励