Enable jumbo frames on iMX8QM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enable jumbo frames on iMX8QM

730件の閲覧回数
Vlongobardi
Contributor II

Hi all,

Do you know if it is possible to enable Jumbo Frames on iMX8QM, and if yes, how could I do that?

The Atheros AR8031-al1b datasheet says that it supports Jumbo Frame up to 10 kB https://www.application-datasheet.com/pdf/qualcomm/ar8031-al1b.pdf 

But executing "ip -d link list" maxmtu is 1966 byte

On the iMX8MPlus documentation (11.7.6.1.2.3) I read that the ENET_QOS memory map has a register, MAC Configuration Register, which has a bit (bit 16, JE) that have to be asserted to enable Jumbo Frames. Do you know if iMX8QM has something similar? How I suppose to assert that bit eventually?

Thanks,

Vincenzo

0 件の賞賛
返信
3 返答(返信)

712件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

686件の閲覧回数
Vlongobardi
Contributor II

Hi, thank you for your reply.

Do you know whether I have to modify the if_ether.h file and build it again or I just have to modify the file?

Unfortunately the latter didn't work for me.

0 件の賞賛
返信

674件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信