Enable jumbo frames on iMX8QM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Enable jumbo frames on iMX8QM

737 次查看
Vlongobardi
Contributor II

Hi all,

Do you know if it is possible to enable Jumbo Frames on iMX8QM, and if yes, how could I do that?

The Atheros AR8031-al1b datasheet says that it supports Jumbo Frame up to 10 kB https://www.application-datasheet.com/pdf/qualcomm/ar8031-al1b.pdf 

But executing "ip -d link list" maxmtu is 1966 byte

On the iMX8MPlus documentation (11.7.6.1.2.3) I read that the ENET_QOS memory map has a register, MAC Configuration Register, which has a bit (bit 16, JE) that have to be asserted to enable Jumbo Frames. Do you know if iMX8QM has something similar? How I suppose to assert that bit eventually?

Thanks,

Vincenzo

0 项奖励
回复
3 回复数

719 次查看
joanxie
NXP TechSupport
NXP TechSupport
0 项奖励
回复

693 次查看
Vlongobardi
Contributor II

Hi, thank you for your reply.

Do you know whether I have to modify the if_ether.h file and build it again or I just have to modify the file?

Unfortunately the latter didn't work for me.

0 项奖励
回复

681 次查看
joanxie
NXP TechSupport
NXP TechSupport
0 项奖励
回复