Does i.MX6 support hardware acceleration for SDL2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does i.MX6 support hardware acceleration for SDL2

968 Views
charleshuang
Senior Contributor II

!Hi,

 

I add libsdl2 to my target rootfs(Yocto) , and use one little test program to test cpu loading, it is almost 80%, so is there any hardware acceleration for SDL2 or not ?

 

Best Regards

 

Original Attachment has been moved to: test1.cpp.txt.zip

Labels (2)
0 Kudos
3 Replies

510 Views
igorpadykov
NXP Employee
NXP Employee

Hi charles

there is no i.MX6 SDL2 hardware acceleration.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

510 Views
charleshuang
Senior Contributor II

Hi igor,

one more question, how about SDL1 ? is it still not h/w acceleration?

Best Regards

0 Kudos

510 Views
igorpadykov
NXP Employee
NXP Employee

Hi charles

there is no SDL1 acceleration.

~igor