Does i.MX287 supports PWM inputs?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does i.MX287 supports PWM inputs?

539件の閲覧回数
sourabhzunke090
Contributor I

How do we read digital pulses from encoders which can have a frequency range 1Hz to 15KHz on i.mx287. The reference manual for i.mx287 has information about the PWM output pins and doesn't mentions anything about reading PWM inputs. Does i.mx287 cannot read PWM inputs.

What is the possible solution to read PWM inputs if i.mx287 doesn't supports it?

Can it be done using HSADC?

Does other SoM in i.MX series support PWM inputs? 

Can I read PWM inputs of the specified range using external peripherals which gives output understandable to i.MX287?

ラベル(4)
タグ(2)
0 件の賞賛
返信
1 返信

414件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi sourabh

please check Chapter 23 Timers and Rotary Decoder (TIMROT)

i.MX28 Reference Manual

http://cache.freescale.com/files/dsp/doc/ref_manual/MCIMX28RM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------