Does NXP provide any stable and bugfix updates to BSP kernel?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does NXP provide any stable and bugfix updates to BSP kernel?

559 Views
krzysztof_kozlo
Contributor II

Hi,

I am using i.MX 8M Mini with a v4.19 kernel from NXP/Codeaurora (imx_4.19.35_1.1.0). It's a pretty old release (v4.19.35) from v4.19 stable tree with a lot of unfixed bugs. The current v4.19 kernel is v4.19.130, so almost 100 stable releases further.

These stable releases come with a lot less and more important bug fixes (including security fixes).

The question: Do you plan to provide BSP v4.19 kernel updated to latest stable v4.19 (e.g. v4.19.130) or you expect every customer should perform such important maintenance by himself?

Best regards,

Krzysztof

Labels (2)
0 Kudos
1 Reply

507 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The latest BSP update is the L5.4.3 and you can download from the code aurora as well. there is no any update from the L4.19.35.

Regards

0 Kudos