Do you support DPRAM in IMX6DualLite?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do you support DPRAM in IMX6DualLite?

607 Views
mingyue-liu
Contributor I

Hi, we want to use the HMS product anybus in the I.MX6 DualLite SOC.

From anybus datasheet, we saw that the anybus have a DPRAM to exchange data with imx6, and we should use parallel addr/data bus from anybus's DPRAM to connect to the imx6.

So, do the imx6 support DPRAM? if yes, how to support it?

the anybus's datasheet is at the attachment.

0 Kudos
2 Replies

498 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

You can reffer to the thread https://community.nxp.com/message/854790 

Have a nice day

Rita

0 Kudos

498 Views
mingyue-liu
Contributor I

Hello Rita,

Thankyou for reply.

Do you mean that we can use EIM to connect to the DPRAM which is in anybus?

The DPRAM which is in anybus is 4Kbytes, 12 address lines, 8 data lines, with OE, RW, CE control lines.

the EIM only support 8/16/32 address lines, so which lines could we choose?

and there no CE line in the EIM

0 Kudos