Demo for MCIMX6Q-SDB and MCIMX-LVDS1 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Demo for MCIMX6Q-SDB and MCIMX-LVDS1 ?

790 Views
tj5
Contributor I

I have MCIMX6Q-SDB board and MCIMX-LVDS1 display. I want to run Linux demo to test it.

On website I see many demo packages for i.MX 6Quad, which will be most suitable for my hardware ?

 

 

I'm testing

Source Code Download Steps Documentation and Demo Images (REV L3.10.17_1.0.0)

in log I see

No panel detected: default to Hannstar-XGA

Display: Hannstar-XGA (1024x768)

and my LCD is black

Original Attachment has been moved to: log.txt.zip

Labels (2)
0 Kudos
2 Replies

562 Views
art
NXP Employee
NXP Employee

Have you connected your LVDS panel to the correct LVDS port? Please check.

Also, refer to the "video" section on the Page 10 of the attached document for the information on how to set up various display ports including LVDS in the kernel command line.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

562 Views
tj5
Contributor I

Thank you for reply, now my LCD is working correctly

0 Kudos