DO254 compliance support for IMX6/IMX8 processors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DO254 compliance support for IMX6/IMX8 processors

871 Views
sarath831989
Contributor I

Hi i am planning to use IMX6/IMX8 series processor in aero design. I need to know whether the processor is complied to DO254 or is there any reference where the processor being used in aero based design earlier. 

Also, is it possible for NXP to provide support to comply the processor with DO-254 standard. 

Tags (1)
0 Kudos
1 Reply

632 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello  Sarath Babu Govinda Babu,

Some i.MX Processors part numbers comply with Automotive or Industrial standards, which may overlap with the requirements for airborne electronic hardware.

There is a document that lists some of the recommendations for these applications:

Freescale Recommendations for Avionic and Defense Applications

https://community.nxp.com/docs/DOC-104735

If you have any doubts about a specific requirement I would recommend contacting your FAE or Distributor for more detailed information.

I hope this helps!

Regards,

0 Kudos