Current limit function of LDO_1P1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Current limit function of LDO_1P1

跳至解决方案
1,490 次查看
takayuki_ishii
Contributor IV

Hello community,

About VDDHIGH_IN voltage of SABRE_SD i.MX6Q board,

It will dropped while wake from deep sleep mode.

  (SABRE_SD_ILIMIT_disable_2P5_1P1_180518_224516_wakeup.png)

It seems that in-rush current to charge a bulk capacitor of NVCC_PLL_OUT.

So enabled current limit of LDO_1P1 by setting PMU_REG_1P1[ENABLE_ILIMIT] bit,

it seems that in-rush current is limited and voltage drop down has been resolved.

  (SABRE_SD_ILIMIT_disable_2P5_enable_1P1_180518_225336_wakeup.png)

But lamp up of NVCC_PLL_OUT is slower than disable of current limit.

Is it OK to use a current limit function while wake up from deep sleep mode?

[Test environment]

Board : SABRE-SD i.MX6Q

OS : Linux BSP 4.9.11_1.0.0

Probe point : 

 ch1 : sh17 (VDDHIGH_IN)

 ch2 : sh17 (VDDHIGH_IN)

 ch3 : SW1_1 (CPUPWRON)

 ch4 : R208 (NVCC_PLL_OUT)

Deep Sleep Mode : 

 Use a configuration of 5.2 Deep Sleep Mode (LPM6) in AN4509.

Best regards,

Ishii.

标签 (3)
0 项奖励
1 解答
1,296 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

>VDDHIGH_IN voltage of SABRE_SD i.MX6Q board,

>It will dropped while wake from deep sleep mode

for VDDHIGH_IN voltage drop, may be useful to check comments on Sabre SD schematic

pastedImage_1.jpg

>Is it OK to use a current limit function while wake up from deep sleep mode?

yes, however additional time for slower ramp should be accounted in CCM_CLPCR

register STBY_COUNT settings, described in sect.18.6.18 CCM Low Power Control Register (CCM_CLPCR).

Procedure for exiting low power mode is described in sect.18.5.3.3.2 Exiting STOP

mode i.MX6DQ Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
4 回复数
1,297 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

>VDDHIGH_IN voltage of SABRE_SD i.MX6Q board,

>It will dropped while wake from deep sleep mode

for VDDHIGH_IN voltage drop, may be useful to check comments on Sabre SD schematic

pastedImage_1.jpg

>Is it OK to use a current limit function while wake up from deep sleep mode?

yes, however additional time for slower ramp should be accounted in CCM_CLPCR

register STBY_COUNT settings, described in sect.18.6.18 CCM Low Power Control Register (CCM_CLPCR).

Procedure for exiting low power mode is described in sect.18.5.3.3.2 Exiting STOP

mode i.MX6DQ Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
1,296 次查看
takayuki_ishii
Contributor IV

Hello Igor,

Thank  you for your quick response.

By attached waveform, a time of NVCC_PLL_OUT that voltage is ready are almost 440usec.

If it must wait more than 440usec as examples, 

   CKIL = 32.768KHz => 30.5usec period

   440usec / 30.5usec = 14.42

to wait more than equal 15CKIL clock cycle so,

  CCM_CGPR[PMIC_DELAY_SCALER] = 0 // clock is not divided

  CCM_CLPCR[STBY_COUNT] = 11b // CCM will wait (15*pmic_delay_scaler)+1 ckil clock cycles = 16 CKIL clock cycle

or

  CCM_CGPR[PMIC_DELAY_SCALER] = 1 // clock is divided /8

  CCM_CLPCR[STBY_COUNT] = 01b // CCM will wait (3*pmic_delay_scaler)+1 ckil clock cycles = 25 CKIL clock cycle

  

Is it correct?

By the way, I found that  NVCC_PLL_OUT and VDDHIGH_CAP are used 22uF for SABRE-SD board.

But these are requested to connect 10uF or small one in IMX6DQ6SDLHDG.

It seems a root cause of VDDHIGH_IN voltage drop down.

Is it OK to use 22uF capacitor?

Best regards,

Ishii.

0 项奖励
1,296 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

provided my answer was just general recommendation.

i.MX6Q Sabre SD board works well with NXP BSPs described on

i.MX Software|NXP 

It is not recommended to change software and hardware configuration

for NVCC_PLL_OUT, as these are verified and work fine.

If customer wishes to proceed with own configuration suggest to use help

with Professional Services to have more detailed analysis and verification:
http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE

Best regards
igor

0 项奖励
1,296 次查看
takayuki_ishii
Contributor IV

Hello Igor,

Thank you for your answer.

I understand your suggestion.

We will introduce my customer to use professional support if they need more verification

about their custom setting.

Best regards,

Ishii.

0 项奖励