Hi,
I'm using an iMX8 processor and linux 5.15 built with yocto.
Currently I've managed to bring up two displays via LVDS and MIPI.
When I list the displays, it shows they are named XWAYLAND0 and XWAYLAND1. I've named them HDMI-A-1 and HDMI-A-2 in the weston.ini file.
I am able to execute two qt applications in two displays if I do that via the weston terminals inside the respective displays.
But can I control in which display the output of an application will be shown if I'm executing them via the debug terminal or using autoboot
Thanks in advance