Configure i.MX6 DualLite as i.MX6 Solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configure i.MX6 DualLite as i.MX6 Solo

Jump to solution
1,370 Views
mahi
Contributor IV

Hello community,

the description of RDIMX6SABREAUTO says "i.MX 6Quad and i.MX 6Dual Lite can be configured as an i.MX 6Dual and i.MX 6Solo processor for lower CPU load applications".

As we are planning a project with i.MX6 Solo and there is no suitable SABRE platform for this processor, I would like to know how exactly this works.

Simply by writing the "NUM_CORES" fuse (if it is writable at all)?

The RDIMX6SABREPLAT description does not mention this feature at all, but I expect that there is also the possibility to disable one core... Please correct me if I'm wrong.

Best Regards,

Martin

Labels (3)
0 Kudos
1 Solution
821 Views
igorpadykov
NXP Employee
NXP Employee

Hi Martin

for Solo one needs to add maxcpus=1 this is described

in i.MX_6Dual6Quad_SABRE-SD_Linux_Release_Notes.pdf

included in Doc bundle L3.0.35_4.1.0_LINUX_DOCS .

Also one can look at document About_i.MX6Solo_DL_LinuxBSP.pdf.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
5 Replies
822 Views
igorpadykov
NXP Employee
NXP Employee

Hi Martin

for Solo one needs to add maxcpus=1 this is described

in i.MX_6Dual6Quad_SABRE-SD_Linux_Release_Notes.pdf

included in Doc bundle L3.0.35_4.1.0_LINUX_DOCS .

Also one can look at document About_i.MX6Solo_DL_LinuxBSP.pdf.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
821 Views
mahi
Contributor IV

Thanks for your answer. I hoped, there was something more "low-level" than limiting the number of used CPUs in software.

0 Kudos
821 Views
igorpadykov
NXP Employee
NXP Employee

Hi Martin

processors are identical, except small details

described in document About_i.MX6Solo_DL_LinuxBSP.pdf

Best regards

chip

821 Views
mahi
Contributor IV

Hi chip,

can you give me a hint, where I can find the document About_i.MX6Solo_DL_LinuxBSP.pdf?

It seems not to be part of any Documentation or BSP packages I downloaded yet...

Best Regards

Martin

0 Kudos
821 Views
igorpadykov
NXP Employee
NXP Employee

Hi Martin

I attached file

Best regards

chip