Hi,
I have encountered an issue with Chromium that was build using Yocto Rev: LF6.6.23_2.0.0 for iMX93 EVK (MCIMX93-EVK).
My build scenario:
Added CORE_IMAGE_EXTRA_INSTALL += "chromium-ozone-wayland" to conf/local.conf
DISTRO=fsl-imx-wayland MACHINE=imx93-11x11-lpddr4x-evk source ./imx-setup-release.sh -b ./builddir
bitbake imx-image-multimedia
After deploying the build to iMX93 EVK, chromium crashes with the following output:
chromium --no-sandbox
[0227/174608.541667:ERROR:file_io_posix.cc(144)] open /sys/devices/system/cpu/cpu0/cpufreq/scaling_cur_freq: No such file or directory (2)
[0227/174608.541847:ERROR:file_io_posix.cc(144)] open /sys/devices/system/cpu/cpu0/cpufreq/scaling_max_freq: No such file or directory (2)
Segmentation fault (core dumped)
Anyone encountered a similar problem, any idea how to fix this issue?
Chromium runs OK when built with Yocto LF 6.1.55-2.2.0
Thanks in advance.
Hi @abt,
Thank you for report this issue.
I would like to share the solution from our team.
Please use the following command to run Chromium:
cd /usr/lib/chromium && ./chromium-bin --use-gl=egl --ozone-platform=wayland --disable-features=VizDisplayCompositor --no-sandbox
This command should work to run Chromium successfully on i.MX93 with the BSP version 6.6.23_2.0.0.
Hi @abt,
I tried to replicate the issue and I can confirm that there is a problem when starting Chromium.
I'm checking with the team for a solution.
Thank you for your patience!
Hi @abt,
Thank you for contacting NXP Support!
I will try to replicate the issue and I will contact you as soon as possible.