Change i.MX8M CPU frequency in Uboot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Change i.MX8M CPU frequency in Uboot

1,465件の閲覧回数
yashavanthashet
Contributor V

Hi all,

We are using i.MX8M 4.9.51_ga release with custom board.

Currently in Uboot boot print its showing "CPU:   Freescale i.MX8MQ rev2.0 1300 MHz (running at 800 MHz)"

Even though CPU supports maximum 1.3GHz board runs only in 800MHz in uboot, can we change it to 1.3GHz in uboot?

Thanks in advance.

Regards,

Yashavantha

1 返信

1,028件の閲覧回数
art
NXP Employee
NXP Employee

Uboot itself does not have an option to change the CPU clock frequency. Thus, it starts at the default CPU core clock frequency of 800MHz that can be further changed at the kernel boot stage by the CPUFREQ driver setup. If you need to change the CPU core clock frequency in Uboot, you have to patch the Uboot code. For that purpose, you can use the CPUFREQ driver code as the reference. For details on the driver, please refer to the Section 2.3.3 of the attached document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------