Hello NXP,
Currently i'm working on i.MX 8M Nano EVK Board but while booting from SD Card it's showing error as :-
Can't find PMIC:PCA9450
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3200MTS
Training FAILED
Can you please tell me, from where [ Board's H/W ] this error gets occured ??
Thanks
Nikhil
解決済! 解決策の投稿を見る。
Most likely, you are trying to run wrong image on your board.
Most likely, you have the EVK kit, equipped with 8MNANOD4-CPU CPU board that contains the DDR4 memory and BD71850MWV PMIC by Rohm, but try to run the image, compiled for the X-815LPD4-CPU board that contains LPDDR4 memory and PCA9450 PMIC by NXP. Please double-check.
Best Regards,
Artur
There is no ready-to-use image for the early i.MX8MNano EVK board version within the L5.4.47 BSP. You have to build it by yourself as described below. Or, you can use the pre-built image, included into the L5.4.3 BSP.
Most likely, you are trying to run wrong image on your board.
Most likely, you have the EVK kit, equipped with 8MNANOD4-CPU CPU board that contains the DDR4 memory and BD71850MWV PMIC by Rohm, but try to run the image, compiled for the X-815LPD4-CPU board that contains LPDDR4 memory and PCA9450 PMIC by NXP. Please double-check.
Best Regards,
Artur
The picture you shared confirms my suspicion. You have the 8MNANOD4-EVK board, but most likely try to run the image for the X-815LPD4-CPU board. Please choose the correct image.
Best Regards,
Artur
Hello NXP TechSupport
i.MX 8M Nano EVK
# Solved :-
1] Issue of PMIC has solved by flashing Linux Demo image[ L5.4.3_1.0.0_MX8MN (REV LF_L5.4.3_1.0.0 ) ], having PMIC : BD71850MWV
# Error 1 :-
2] But previously 1 month ago i had tried to flash a Linux Demo Image [ L5.4.24_2.1.0_MX8MN (REV L5.4.24_2.1.0 ) ] but it didn't work at that time, shown can't find PMIC : PCA9450.
# Error 2 :-
3] And after that I had also tried Yocto set up for BSP [ i.MX 8M Nano EVK ] from Yocto project User's Guide [ Rev. L5.4.24_2.1.0, 06/2020 ]
$ DISTRO=fsl-imx-xwayland MACHINE=imx8mnevk source imx-setup-release.sh -b build-xwayland
$ bitbake imx-image-full
After building above image i got all images and flashed on SD Card imx-image-full-imx8mnevk.wic
after successful flashing, getting same error as can't find PMIC : PCA9450.
So, what i should i do for getting correct boot logs with my own Yocto Set up for Nano EVK ??
Thanks
Nikhil
Thanks Artur for your time and kind Support
Issue Solved and now showing power_bd71837_init [ PMIC : BD71837 ] instead of [ PMIC : PCA9450 ] while booting from SD Card.
Thanks
Nikhil
Thank You very much NXPtechSupport
Actually, i'm not understanding how to select perfect image for Nano Board that which is having PMIC [BD71850MWV ] and which is having PMIC [ PCA9450 ].
So, can you please share a link for Linux and Android image for i.MX 8M Nano-D4 [ DDR4 ] having PMIC [ BD71850MWV ] ??
Thanks
Nikhil