Can i.mx6 sabre platform use dual LVDS?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can i.mx6 sabre platform use dual LVDS?

ソリューションへジャンプ
1,715件の閲覧回数
JHY
Contributor IV

Is it possible dual display(LVDS + LVDS) in the sabre platform?

I found it has two LVDS connector and it works fine in single display.

So tell me how to do it in u-boot bootargs please.

ラベル(1)
0 件の賞賛
返信
1 解決策
757件の閲覧回数
saurabh206
Senior Contributor III

Hi

You can used the ldb=dul0 for dual display mode.

Following is different option used for LVDS connection.

"ldb=spl0/1"       --      split mode on DI0/1

"ldb=dul0/1"       --      dual mode on DI0/1

"ldb=sin0/1"       --      single mode on LVDS0/1

"ldb=sep0/1" --      separate mode begin from LVDS0/1

Thanks

Saurabh

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
758件の閲覧回数
saurabh206
Senior Contributor III

Hi

You can used the ldb=dul0 for dual display mode.

Following is different option used for LVDS connection.

"ldb=spl0/1"       --      split mode on DI0/1

"ldb=dul0/1"       --      dual mode on DI0/1

"ldb=sin0/1"       --      single mode on LVDS0/1

"ldb=sep0/1" --      separate mode begin from LVDS0/1

Thanks

Saurabh

0 件の賞賛
返信