Hi Igorpadykov,
Thanks for the reply, but I want to get the clock in CCM_CLK1_P pin expecting 8MHz clock (p17 pin i.mx6ull) what changes (any exact registers & dividers in inside processor) or from 24Mhz external clock source how to get 8Mhz clock inside processor? and connections between CCM_CLK1_P pin(p17) & 24Mhz clock inside IC ?
Hi prahbu
sorry this is not possible as answered on
CCM_CLK1_P clock output 8MHz generating settings
Frequency options given in CCM_ANALOG_MISC1n[LVDS1_CLK_SEL] do not allow
such frequency.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------