Boot i.MX53 QSB from u-boot 2011.12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot i.MX53 QSB from u-boot 2011.12

1,140件の閲覧回数
HenryChiang
Contributor I

Hi

Would that be possible to boot i.MX53 QSB from u-boot 2011.12?

I download u-boot 2011.12 and ELDK5.1 from http://www.denx.de.

I have installed ELDK 5.1 for armv7a first.

I enter u-boot folder to make u-boot.bin and no result come out from console.

Would you please help ?

Thanks

Here is my step.

1.Install ELDK5,1 for armv7a at default folder (/opt/eldk-5.1/armv7a)

2.type "source /opt/eldk-5.1/armv7a/environment-setup-armv7a-vfp-neon-linux-gnueabi"

3.type "export CROSS_COMPILE=arm-linux-gnueabi"

4.make distclean

5.make mx53loco_config

6.make all

7.Using dd to flash u-boot.bin into microSD card and there is no result come out

Thanks for great help

タグ(1)
0 件の賞賛
返信
1 返信

953件の閲覧回数
HenryChiang
Contributor I

HI All

I have find the answer from other discussion.

Please refer to this.

Thanks all help

http://imxcommunity.org/group/bringup-and-build/forum/topics/i-mx53-u-boot-issues

0 件の賞賛
返信