Hi,
I need to build an image for IMX6 Sabre auto. Which would be the best image that can be built using a linux machine? My requirements are that the apt-get command should be working and that the gui should work as well.
1.use fsl-community-bsp to build images (google it)
2.in local.conf add this line
IMAGE_INSTALL_append=" apt-native"
3. enter command
bitbake core-image-x11
Follow these steps thoughtfully, you will get a image precisely as you need without any extra items.
minimal image with gui and apt package manager.
If boot time and image size is not a constraint use a ubuntu rootfs provided by freescale.
Regards,
Piyush Ashtikar
/////////////////////////////////////////////////////////////////////////////////
Please mark answer correct if you find it useful.
////////////////////////////////////////////////////////////////////////////////
Hi Ajay
for ubuntu (using apt-get command) one can check
Installing Ubuntu Rootfs on NXP i.MX6 boards | NXP Community
For ordinary linux one can look at nxp bsp releases located on
================================================================
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------