Aptina MT9P031 on imx53 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Aptina MT9P031 on imx53 ?

Jump to solution
2,008 Views
josa
Contributor II

Hi

I have some micron images sensors : MT9P031 and would like to use these on imx53 .

So before i get to design my pcb i would like to know if someone already used this sensor on the imx53

There seem to be several places in the kernel configuration to enable image sensors

device drivers ->multimedia support -> video capture adapters -> Video for linux Camera ->Mxc camera V4L2

device drivers ->multimedia support -> video capture adapters -> Soc camera support

I found some OV5642 based modules but they are overpriced ...

Thanks in advance.

Johan

Labels (4)
0 Kudos
Reply
1 Solution
1,254 Views
BrilliantovKiri
Senior Contributor I

I think you can use it, but usualy Aptina CMOS have output stream in RAW Bayer format. Because iMX53 codecs work only with YUV and CPU can't convert RAW to YUV you should make it.

View solution in original post

0 Kudos
Reply
2 Replies
1,255 Views
BrilliantovKiri
Senior Contributor I

I think you can use it, but usualy Aptina CMOS have output stream in RAW Bayer format. Because iMX53 codecs work only with YUV and CPU can't convert RAW to YUV you should make it.

0 Kudos
Reply
1,254 Views
haitao
Contributor II

hi:

     i want to know whether imx6q can process the raw rgb data from camera?

0 Kudos
Reply