[Android 4.4.2] Preview and video recording issue on USB camera

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[Android 4.4.2] Preview and video recording issue on USB camera

2,532 次查看
charleshuang
Senior Contributor II

Hi NXP

I test USB camera (logitech webcam) in imx6 sabresd demo board (Android 4.4.2).

I used usb-hub to connect to OTG port. 

Because I need to connect usb camera ,usb mouse and keyboard. 

When I open camera apk and preview it, the picture is not correctly.

Please refer the attachment file.

VID_20160908_090232.3gpp is recording video.

pass.jpg is correct picture.

error.jpg is not correct picture.

Do you have any advice?

Clayder

标签 (2)
0 项奖励
2 回复数

2,312 次查看
SergioSolis
NXP Employee
NXP Employee

Are you having this problem only when you use the USB Hub?, or is it independent of it?

0 项奖励

2,312 次查看
charleshuang
Senior Contributor II

Hi SerigioSolis

Yes, this problem only when I  use the USB HUB.  Because our application need to connect usb camera , usb mouse and usb keyboard in platform.

0 项奖励