Altium Files for IMX8M Nano DDR4 Evalboard

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Altium Files for IMX8M Nano DDR4 Evalboard

3,403 次查看
markushager
Contributor II

Dear Victor, can you please send Altium Files for 8MNANOD4-EVK to th FTP account I sent you via email?

标签 (1)
14 回复数

2,644 次查看
Sal2020
Contributor II

0

标记 (2)

3,105 次查看
Ronak05
Contributor I

Hello NXP Techsupport Team,

 

I have been trying to import the design files for i.MX 8M Nano EVK  in Altium19 but while importing the files altium displays the error of files being old or unrecognized file type. 

 

Can you please email me the latest version altium files of this Eval kit ?

 

My email id is ronakk@acevin.com

0 项奖励

3,184 次查看
b36401
NXP Employee
NXP Employee

ftp> put 8MNDDR4.tar
local: 8MNDDR4.tar remote: 8MNDDR4.tar
200 PORT command successful
150 Opening BINARY mode data connection for 8MNDDR4.tar
226 Transfer complete
2600960 bytes sent in 4.09 secs (620.6434 kB/s)
ftp>

3,184 次查看
markushager
Contributor II

Thank you for the files!

0 项奖励

3,184 次查看
radias
Contributor II

Hi Markus,

Could you send me these files (Altium) in my email please?

radias@inatel.br

Thank you in advance.

0 项奖励

3,184 次查看
carlesre
Contributor II

Hi Ricardo,

could you send me these 8MNANOD4-EVK Altium files?

carles.recasens@wallbox.com

I would really appreciate that!

Thank you in advance

Carles

0 项奖励

3,188 次查看
radias
Contributor II

Hi Carles,

Files were sent to your email.

Let me know if they work fine.

Kind Regards.

Ricardo Antonio Dias

email: radias@inatel.br<mailto:radias@inatel.br> | skype: dias.a.ricardo

Tel: (35) 3471-9914 | ramal: 914

Antes de imprimir, pense em sua responsabilidade com o meio ambiente!

De: carlesre <admin@community.nxp.com>

Enviada em: sexta-feira, 5 de junho de 2020 11:54

Para: Ricardo Antonio Dias <radias@inatel.br>

Assunto: Re: - Re: Altium Files for IMX8M Nano DDR4 Evalboard

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Altium Files for IMX8M Nano DDR4 Evalboard

reply from Carles Recasens<https://community.nxp.com/people/carlesre?et=watches.email.thread> in i.MX Processors - View the full discussion<https://community.nxp.com/message/1322510?commentID=1322510&et=watches.email.thread#comment-1322510>

3,188 次查看
carlesre
Contributor II

Hi Ricardo,

I have received Altium files, they seem to be OK.

Thank you very much, I really appreciate your support!!

If I can help you with something, please let me know

Kind Regards,

Carles

0 项奖励

3,186 次查看
radias
Contributor II

Hi Carles,

Great to hear that.

Good to know that I have some on to help me if a I were in trouble.

Kind Regards,

Ricardo Antonio Dias

email: radias@inatel.br<mailto:radias@inatel.br> | skype: dias.a.ricardo

Tel: (35) 3471-9914 | ramal: 914

Antes de imprimir, pense em sua responsabilidade com o meio ambiente!

De: carlesre <admin@community.nxp.com>

Enviada em: segunda-feira, 8 de junho de 2020 04:10

Para: Ricardo Antonio Dias <radias@inatel.br>

Assunto: Re: - Re: Altium Files for IMX8M Nano DDR4 Evalboard

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Altium Files for IMX8M Nano DDR4 Evalboard

reply from Carles Recasens<https://community.nxp.com/people/carlesre?et=watches.email.thread> in i.MX Processors - View the full discussion<https://community.nxp.com/message/1323052?commentID=1323052&et=watches.email.thread#comment-1323052>

0 项奖励

3,186 次查看
radias
Contributor II

Hi Markus,

I'd like to ask you if you have de base board files to IMX8M Nano able to be imported into Altium also?

May you can send me this files?

Thank you in advance.

Best regards.

Ricardo Dias.

0 项奖励

3,186 次查看
radias
Contributor II

Hi Markus,

Thanks for sent files.

I already test them and they are all ok.

Best Regards,

Ricardo Dias.

0 项奖励

3,186 次查看
b36401
NXP Employee
NXP Employee

I just sent you the files.

0 项奖励

3,066 次查看
kbrakora
Contributor I

Hi Victor,

Could I get the Altium project files or the files in a format importable into Altium?  My e-mail address is kbrakora@btengin.com.

Best Regards,

Karl

0 项奖励

3,040 次查看
Yuri
NXP Employee
NXP Employee

@kbrakora 
Hello,

   it makes sense to create separate thread or request:

 

https://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu

 

Regards,
Yuri.

0 项奖励