About the SDXC support on Android4.4.2 with MX6Q_SABRE-SDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About the SDXC support on Android4.4.2 with MX6Q_SABRE-SDB

678件の閲覧回数
yuuki
Senior Contributor II

Dear all,

Our customer runs Android4.4.2 on MX6Q-SABRE-SDB.

A SDXC card is mounted on Android4.4.2.

Howevwer, it is recognized as 0 GB.
And the contents of SDXC cannot be seen.

Does Android4.4.2_BSP of FSL support SDXC?


Best Regards,
Yuuki

ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

538件の閲覧回数
yuuki
Senior Contributor II

A SDXC card is connected to a USB OTG port through a SD-USB adapter.
This SD-USB adapter corresponds to USB3.0.

It is recognized as 0 GB and the contents of SDXC cannot be seen.
If it is unmounted and then mounted, it is mounted correctly and the contents can be seen.


If the SD-USB adapter of USB2.0 correspondence is used, this problem will not occur.

Is this a problem of a SD-USB adapter?

Best Regards,
Yuuki

0 件の賞賛
返信

538件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Yuuki,

The 3.0 usb adapter could be the reason. Have you tried this adapter in the linux host?, can you check it and see what happens?

0 件の賞賛
返信