About the SDXC support on Android4.4.2 with MX6Q_SABRE-SDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the SDXC support on Android4.4.2 with MX6Q_SABRE-SDB

675 Views
yuuki
Senior Contributor II

Dear all,

Our customer runs Android4.4.2 on MX6Q-SABRE-SDB.

A SDXC card is mounted on Android4.4.2.

Howevwer, it is recognized as 0 GB.
And the contents of SDXC cannot be seen.

Does Android4.4.2_BSP of FSL support SDXC?


Best Regards,
Yuuki

Labels (1)
0 Kudos
Reply
2 Replies

535 Views
yuuki
Senior Contributor II

A SDXC card is connected to a USB OTG port through a SD-USB adapter.
This SD-USB adapter corresponds to USB3.0.

It is recognized as 0 GB and the contents of SDXC cannot be seen.
If it is unmounted and then mounted, it is mounted correctly and the contents can be seen.


If the SD-USB adapter of USB2.0 correspondence is used, this problem will not occur.

Is this a problem of a SD-USB adapter?

Best Regards,
Yuuki

0 Kudos
Reply

535 Views
SergioSolis
NXP Employee
NXP Employee

Hello Yuuki,

The 3.0 usb adapter could be the reason. Have you tried this adapter in the linux host?, can you check it and see what happens?

0 Kudos
Reply