About i.MX6 Internal LDO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About i.MX6 Internal LDO

Jump to solution
2,251 Views
okamotosatoshi
Contributor IV

Hello.

I want to check about i.MX6Q.

Thank you to answer the following questions.

We have created a custom board of i.MX6Q.

I confirmed the voltage drop in VDDSOC_CAP at startup.

I attach the measured waveform. (VDDSOC_CAP : No load)

CH1:5V(Power-supply voltage)

CH2:2.5V(VDDHIGH_CAP)

CH3:1.1V(VDDSOC_CAP)

CH4:POR_B

capture1.png

Is there a way to avoid the voltage drop of VDDSOC_CAP ?

In addition, the voltage drop of VDDSOC_CAP was Would no issue ?

Start-up failure has occurred on the SATA boot.

Believes that the above reason.

(For reset release timing occurred voltage drop of VDDSOC_CAP.)

Regards,

-satoshi

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,485 Views
igorpadykov
NXP Employee
NXP Employee

Hi okamoto

in general there is nothing wrong in these

waveforms. Transients and glitches are allowed,

during this time POR should be asserted.

①VP power supply is no issue using VDDSOC_CAP?

No issue.

②Are there any plans to improve this issue ?

No plans, because it is allowed.

③This phenomenon will not occur in SABRE Board?

SABRE Board may have incorrect waveforms because it was designed

in time when i.MX6 datasheets were not finalized.

Best regards

chip

View solution in original post

0 Kudos
Reply
5 Replies
1,485 Views
okamotosatoshi
Contributor IV

Hi, chip

Thank you for reply.

I was relieved at the fact that no problem waveform.

It was confirmed to I get information, but would not be applicable items.

I confirmed the similar symptoms in other substrates.

- incorrect capacitor value on VDDSOC_CAP

A)VDDSOC_CAP have placed more than capacitor of 22uF.

 No change If you place a 100uF.

- incorrect current capability on VDDSOC_IN from PMIC

- incorrect power-up sequence

A)There is no problem because you have the power generated by the PMIC.

 (As with SABRE Board.)

If you 100uF capacitor , the voltage at the first time is reduced.

Thereafter , it is a normal voltage rise for the second time.

(Discharge curve becomes gentle.)

From the above , I believe the rise of the first time that he crowded around the power of other i.MX6.

After that , it seems to be a constant load discharge.(Measured values with the calculated values match almost.)

I believe the rise of the second is correct output voltage of the LDO.

I think the issue i.MX6 series.

Are there any plans to improve this problem ?

This phenomenon will not occur in SABRE Board?

CPU:MCIMX6Q5EYM10AC

PMIC:MMPF0100F0AEP

Regards,

-satoshi

0 Kudos
Reply
1,485 Views
okamotosatoshi
Contributor IV

Hi, chip

I will append the contents measured .

Please refer to the attached document for details.

・VDDSOC_CAP/VDDPU_CAP wraps around VDDHIGH_IN is supplied.

・When VDDHIGH_IN turn off, LDO is not outputted.

 (VDDHIGH_IN enabled internal LDO?)

・Rising edge of the second time changes.(VDDSOC_CAP/VDDPU_CAP)

 (You are shifting inside the output timing ?)

・Rising edge of the first have the same timing.(VDDSOC_CAP/VDDPU_CAP)

From the above, I believe that wraps around from VDDHIGH_IN.

①VP power supply is no issue using VDDSOC_CAP?

②Are there any plans to improve this issue ?

③This phenomenon will not occur in SABRE Board?

Regards,

-satoshi

0 Kudos
Reply
1,486 Views
igorpadykov
NXP Employee
NXP Employee

Hi okamoto

in general there is nothing wrong in these

waveforms. Transients and glitches are allowed,

during this time POR should be asserted.

①VP power supply is no issue using VDDSOC_CAP?

No issue.

②Are there any plans to improve this issue ?

No plans, because it is allowed.

③This phenomenon will not occur in SABRE Board?

SABRE Board may have incorrect waveforms because it was designed

in time when i.MX6 datasheets were not finalized.

Best regards

chip

0 Kudos
Reply
1,485 Views
okamotosatoshi
Contributor IV

Hi, chip

Thank you for reply.

I will assert POR during the waveform.

Thank you for information.

Asserting the POR until normal operation.

Then use it to reset release.

Best regards

-satoshi

0 Kudos
Reply
1,485 Views
igorpadykov
NXP Employee
NXP Employee

Hi okamoto

in general there is nothing wrong in these

waveforms.

VDDSOC_CAP sag may be caused by several reasons:

- incorrect power-up sequence

- incorrect capacitor value on VDDSOC_CAP

- incorrect current capability on VDDSOC_IN from PMIC

Please check all above with Chapter 2 Design Checklist,

Chapter 4 Requirements for Power Management,

Chapter 8 Avoiding Board Bring-up Problems

IMX6DQ6SDLHDG IMX6DQ6SDLHDG, Hardware Development Guide

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply