About audio: how do I ensure which internal aux port is used

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About audio: how do I ensure which internal aux port is used

1,092 Views
kainanzhu
Contributor I

Hi NXP:

   I'm now porting audio. I used external  aux port is aux3 from Schematic, but I don't know which internal port is used.

   How do I ensure which internal aux port is used?

  

Thanks.

0 Kudos
Reply
7 Replies

952 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Are you using one of our boards? If yes, Which one?

Best Regards,

Diego.

0 Kudos
Reply

952 Views
kainanzhu
Contributor I

Hi:

   Yes, I use imx6q.

Thanks

0 Kudos
Reply

952 Views
kainanzhu
Contributor I

Yes. I'm using the SABRESD board

0 Kudos
Reply

952 Views
diegoadrian
NXP Employee
NXP Employee

Hello

Like you said, according to the schematic, the external aux port is connected to aud3 port. But following the schematic that audio port is connected to the CSI0_DAT (4 - 7) of the i.MX6Q - DISP CSI. Confirming with the i.MX pins tool the CSI0_DAT (4 - 7) is muxed with the AUD3_TXC, AUD3_TXD, AUD3_TXFS, AUD3_RXD respectively.

I hope this can solve your question.

Best Regards,

Diego.

0 Kudos
Reply

952 Views
diegoadrian
NXP Employee
NXP Employee

Hello

Are you using the SABRESD board?

Best Regards,

Diego.

0 Kudos
Reply

952 Views
kainanzhu
Contributor I

Hi Vaverka:

   we use imx6qdl.

Thanks.

0 Kudos
Reply

952 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Kainan,

Could you please specify which NXP IC are you using? It will help us to find the correct space for your question.

Best regards,

Tomas

0 Kudos
Reply