About Out of Reset Condition of ENET1_RX_DATA0(F16)pin of i.MX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About Out of Reset Condition of ENET1_RX_DATA0(F16)pin of i.MX6UL

Jump to solution
846 Views
yuuki
Senior Contributor II

I have a question about Out of Reset Condition of ENET1_RX_DATA0(F16)pin of i.MX6UL.

I seem that the description of Datasheet is different from register explanation of Reference Manual.

In Datasheet,
The Out of Reset Condition of ENET1_RX_DATA0(F16)pin is ALT5/ENET1_RX_DATA0.

ENET1_RX_DATA0_UL_Datasheet.png

In Reference Manual,
The Reset value of MUX_MODE field in IOMUXC_SW_MUX_CTL_PAD_ENET1_RX_DATA0 register is "ALT5 mux port: GPIO2_IO00".

ENET1_RX_DATA0_UL_RM.png

Which description is correct?

Best Regards,
Yuuki

Labels (1)
0 Kudos
1 Solution
680 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

The datasheet is not correct, that pin's default function is ALT5, GPIO2_IO00, not ENET1_RX_DATA0.

View solution in original post

0 Kudos
2 Replies
680 Views
art
NXP Employee
NXP Employee

The correct value is the ALT5 GPIO2_IO00 value, as described in the Reference Manual document. The ALT0 value, given in the Data Sheet document, is just a typo.


Have a great day,
Artur

681 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

The datasheet is not correct, that pin's default function is ALT5, GPIO2_IO00, not ENET1_RX_DATA0.

0 Kudos