About MMDC PHY Read DQS Gating Control Register in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About MMDC PHY Read DQS Gating Control Register in i.MX6DQ.

Jump to solution
1,441 Views
keitanagashima
Senior Contributor I

Dear All,

I have a question about DDR setting register.

My customer would like to use DDR3_x64.

Refer to 44.12.46 MMDC PHY Read DQS Gating Control Register 0 (MMDCx_MPDGCTRL0) in MCIMX6DQRM(Rev.2).

There is below description.

======

For Channel 0: DDR3_x16, DDR3_x32, DDR3_x64

For Channel 1: DDR3_x64

======

Next, refer to "DG_HC_DEL1" bits.

-----------

Read DQS gating half cycles delay for Byte1 (channel 0 register) and Byte5 in 64-bit mode (channel 1 register)

-----------

Last, refer to "DG_CMP_CYC" and "DG_DIS" bit ,etc.

There isn't the description of channel 0 and channel 1.

[Question]

How should one set channel 0 and channel 1 to MMDCx_MPDGCTRL0?

I couldn't understand well...

Best Regards,

Keita

Labels (3)
0 Kudos
Reply
1 Solution
1,136 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita,

>DG_HC_DEL1 and DG_HC_DEL0 bits were set for Channel 0 & 1 PHY?


Yes.


>Refer to Figure 2. DDR3 64-Bit Calibration Registers in AN4476(Rev.2).

>I have understood that MMDCx_MPDGCTRL0 register is "Calibration control" which is in Figure.2.

I think Figure 2 just shows generic structure, not registers.

Best regards

igor

View solution in original post

0 Kudos
Reply
7 Replies
1,136 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

DQS Gating is used only for DDR3 memory, only channel 0 is used.

I.MX6Q has two “logic controllers” – one controller for each “channel”

or AXI port - this is not relevant for DDR3, only for LPDDR2.

Channel 1 ‘logic controller’ only employed when configuring MMDC for

dual-channel LPDDR2 usage and not used for DDR3.

Channel 0 , 1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,136 Views
keitanagashima
Senior Contributor I

Hi Igor,

Thank you for your reply.

Sorry, I couldn't understand well.

Let me clarify these registers again.

My customer will use DDR3 with x64 bits width.

Refer to 44.12.46 MMDC PHY Read DQS Gating Control Register 0 (MMDCx_MPDGCTRL0) in MCIMX6DQRM(Rev.2).

Are these below description typo??


1. Supported Mode Of Operations:

======

For Channel 0: DDR3_x16, DDR3_x32, DDR3_x64

For Channel 1: DDR3_x64

======

2. DG_HC_DEL1 and DG_HC_DEL0 bits

======

Read DQS gating half cycles delay for Byte1 (channel 0 register) and Byte4 in 64-bit mode (Channel 1 register)

======

Best Regards,

Keita

0 Kudos
Reply
1,136 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita,

sorry, I couldn't understand well:

where so you think typo - what word exactly?


Best regards

igor


0 Kudos
Reply
1,136 Views
keitanagashima
Senior Contributor I

Hi Igor,

You answered; DQS Gating is used only for DDR3 memory, only channel 0 is used.

So I consider that below description looks typo.

1. Supported Mode Of Operations:

======

For Channel 0: DDR3_x16, DDR3_x32, DDR3_x64

For Channel 1: DDR3_x64

======

2. DG_HC_DEL1 and DG_HC_DEL0 bits

======

Read DQS gating half cycles delay for Byte1 (channel 0 register) and Byte4 in 64-bit mode (Channel 1 register)

======

Best Regards,

Keita

0 Kudos
Reply
1,136 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita,

thanks for clarifcation.

This is not accurate wording, since there are

two logic terms (please look at image above):

1. Channel1 logic controller

2. Channel1 PHY

meaning in text was for "Channel1 PHY" - configuration

characteristics for data bytes [4-7]


Best regards

igor

0 Kudos
Reply
1,136 Views
keitanagashima
Senior Contributor I

Hi Igor,

Thank you for your reply.

i.e. DG_HC_DEL1 and DG_HC_DEL0 bits were set for Channel 0 & 1 PHY?

Refer to Figure 2. DDR3 64-Bit Calibration Registers in AN4476(Rev.2).

I have understood that MMDCx_MPDGCTRL0 register is "Calibration control" which is in Figure.2.

Best Regards,

Keita

0 Kudos
Reply
1,137 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita,

>DG_HC_DEL1 and DG_HC_DEL0 bits were set for Channel 0 & 1 PHY?


Yes.


>Refer to Figure 2. DDR3 64-Bit Calibration Registers in AN4476(Rev.2).

>I have understood that MMDCx_MPDGCTRL0 register is "Calibration control" which is in Figure.2.

I think Figure 2 just shows generic structure, not registers.

Best regards

igor

0 Kudos
Reply