AR6000: SDIO bus operation failed! MMC stack returned : -84 ,what the means of SDIO -84 and how to solved or avoid it

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AR6000: SDIO bus operation failed! MMC stack returned : -84 ,what the means of SDIO -84 and how to solved or avoid it

3,378 次查看
junjie_tan
Contributor I
U-Boot 2018.03 (Apr 17 2020 - 09:12:47 +0800)
CPU:   Freescale i.MX8QXP revB A35 at 1200 MHz at 30C
Model: Freescale i.MX8QXP MEK
Board: iMX8QXP MEK
Boot:  MMC0
DRAM:  3 GiB
VService: Connection is ok on MU mu@5d230000
TCPC:  Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]
MMC:   priv->vs18_enable = 1
caps_test = 0x2000780b
priv->vs18_enable = 1
caps_test = 0x2000780b
FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... esdhc_set_voltage error -5
esdhc_set_voltage error -5
*** Warning - bad CRC, using default environment
Failed (-5)
[pcie_ctrlb_sata_phy_init_rc] LNK DOWN 8600000
In:    serial
Out:   serial
Err:   serial
 BuildInfo:
  - SCFW f83a2bed, SECO-FW 92ef1143, IMX-MKIMAGE 0d258881, ATF
  - U-Boot 2018.03
flash target is MMC:0
esdhc_set_voltage error -5
esdhc_set_voltage error -5
Net:  
Warning: ethernet@5b040000 using MAC address from ROM
eth0: ethernet@5b040000 [PRIME]
Warning: ethernet@5b050000 (eth1) using random MAC address - ae:8f:fb:ff:a6:c0
, eth1: ethernet@5b050000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot:  0
 verify OK, boot 'boot_a'
Kernel load addr 0x80280000 size 30837 KiB
kernel   @ 80280000 (31576576)
ramdisk  @ 83400000 (7425863)
fdt      @ 83200000 (83332)
## Flattened Device Tree blob at 83200000
   Booting using the fdt blob at 0x83200000
   Using Device Tree in place at 0000000083200000, end 0000000083217583
Disable gpt0@5d140000, resource id 207 not owned
/dma-controller@591F0000, 61944
/dma-controller@599F0000, 62832
/dma-controller@5a1f0000, 61068
/dma-controller@5a1f0000, 61068
Starting kernel ...
[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 4.14.98 (camel@sznfore-dell) (gcc version 4.9.x 20150123 (prerelease) (GCC)) #2 SMP PREEMPT Thu Apr 16 10:00:26 CST 2020
[    0.000000] Boot CPU: AArch64 Processor [410fd042]
[    0.000000] Machine model: Freescale i.MX8QXP MEK
[    0.000000] earlycon: lpuart32 at MMIO 0x000000005a060000 (options '115200')
[    0.000000] bootconsole [lpuart32] enabled
[    0.000000] efi: Getting EFI parameters from FDT:
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created DMA memory pool at 0x0000000090400000, size 8 MiB
[    0.000000] OF: reserved mem: initialized node rpmsg_dma@0x90400000, compatible id shared-dma-pool
[    0.000000] Reserved memory: ION carveout pool at 0x00000000f8000000, size 128 MiB
[    0.000000] OF: reserved mem: initialized node imx_ion@0, compatible id imx-ion-pool
[    0.000000] cma: Reserved 800 MiB at 0x00000000ae000000
[    0.000000] NUMA: No NUMA configuration found
[    0.000000] NUMA: Faking a node at [mem 0x0000000000000000-0x00000008bfffffff]
[    0.000000] NUMA: NODE_DATA [mem 0x8bff7aa80-0x8bff7c87f]
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000080200000-0x00000000ffffffff]
[    0.000000]   Normal   [mem 0x0000000100000000-0x00000008bfffffff]
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000080200000-0x0000000083ffffff]
[    0.000000]   node   0: [mem 0x0000000086200000-0x0000000087ffffff]
[    0.000000]   node   0: [mem 0x0000000088800000-0x000000008fffffff]
[    0.000000]   node   0: [mem 0x0000000090c00000-0x0000000091ffffff]
[    0.000000]   node   0: [mem 0x0000000094c00000-0x00000000ffffffff]
[    0.000000]   node   0: [mem 0x0000000880000000-0x00000008bfffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000080200000-0x00000008bfffffff]
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000] psci: SMC Calling Convention v1.1
[    0.000000] random: get_random_bytes called from start_kernel+0xa8/0x414 with crng_init=0
[    0.000000] percpu: Embedded 25 pages/cpu @ffff80083ff10000 s64536 r8192 d29672 u102400
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] Speculative Store Bypass Disable mitigation not required
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 748552
[    0.000000] Policy zone: Normal
[    0.000000] Kernel command line: console=ttyLP0,115200 earlycon=lpuart32,0x5a060000,115200 init=/init androidboot.hardware=freescale androidboot.fbTileSupport=enable cma=800M@0x960M-0xe00M androidboot.primary_display=imx-drm firmware_class.path=/vendor/etc/firmware transparent_hugepage=never androidboot.console=ttyLP0 buildvariant=userdebug androidboot.serialno=1102680e82963f70 androidboot.btmacaddr=11:02:68:0e:82:96 androidboot.soc_type=imx8qxp androidboot.storage_type=emmc androidboot.boottime=1BLL:0,1BLE:24211499,KL:0,KD:0,AVB:2120,ODT:0,SW:0 androidboot.bootreason=reboot androidboot.verifiedbootstate=green androidboot.slot_suffix=_a dm="1 vroot none ro 1,0 3611944 verity 1 PARTUUID=628e7189-62e6-406e-98b8-41b6a8254a55 PARTUUID=628e7189-62e6-406e-98b8-41b6a8254a55 4096 4096 451493 451493 sha1 2e59d456cdd5c07961943800072d5b4bd7f5a0e5 9c9f947fb565b400d48b47df9b93b2b6099625a7 10 restart_on_corruption ignore_zero_blocks use_fec_from_device PARTUUID=628e7189-62e6-406e-98b8-41b6a8254a55 fe
[    0.000000] device-mapper: init: will configure 1 devices
[    0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
[    0.000000] software IO TLB: mapped [mem 0xf3fff000-0xf7fff000] (64MB)
[    0.000000] Memory: 1945480K/3043328K available (15868K kernel code, 2420K rwdata, 7004K rodata, 5504K init, 523K bss, 278648K reserved, 819200K cma-reserved)
[    0.000000] Virtual kernel memory layout:
[    0.000000]     modules : 0xffff000000000000 - 0xffff000008000000   (   128 MB)
[    0.000000]     vmalloc : 0xffff000008000000 - 0xffff7dffbfff0000   (129022 GB)
[    0.000000]       .text : 0xffff000008080000 - 0xffff000009000000   ( 15872 KB)
[    0.000000]     .rodata : 0xffff000009000000 - 0xffff0000096e0000   (  7040 KB)
[    0.000000]       .init : 0xffff0000096e0000 - 0xffff000009c40000   (  5504 KB)
[    0.000000]       .data : 0xffff000009c40000 - 0xffff000009e9d200   (  2421 KB)
[    0.000000]        .bss : 0xffff000009e9d200 - 0xffff000009f20090   (   524 KB)
[    0.000000]     fixed   : 0xffff7dfffe7f9000 - 0xffff7dfffec00000   (  4124 KB)
[    0.000000]     PCI I/O : 0xffff7dfffee00000 - 0xffff7dffffe00000   (    16 MB)
[    0.000000]     vmemmap : 0xffff7e0000000000 - 0xffff800000000000   (  2048 GB maximum)
[    0.000000]               0xffff7e0000008000 - 0xffff7e0021000000   (   527 MB actual)
[    0.000000]     memory  : 0xffff800000200000 - 0xffff800840000000   ( 33790 MB)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000]  RCU restricting CPUs from NR_CPUS=64 to nr_cpu_ids=4.
[    0.000000]  Tasks RCU enabled.
[    0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: no VLPI support, no direct LPI support
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000051b00000
[    0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[    0.000005] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[    0.011321] Console: colour dummy device 80x25
[    0.015501] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[    0.025681] pid_max: default: 32768 minimum: 301
[    0.030360] Security Framework initialized
[    0.034371] SELinux:  Initializing.
[    0.039179] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes)
[    0.046709] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)
[    0.053459] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes)
[    0.060127] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes)
[    0.083310] ASID allocator initialised with 32768 entries
[    0.096407] Hierarchical SRCU implementation.
[    0.109815] *****Initialized MU
[    0.112669] ***** imx8_init_pm_domains *****
[    0.118041] CPU identified as i.MX8QXP, silicon rev 1.1
[    0.124778] EFI services will not be available.
[    0.137029] smp: Bringing up secondary CPUs ...
[    0.169939] Detected VIPT I-cache on CPU1
[    0.169969] GICv3: CPU1: found redistributor 1 region 0:0x0000000051b20000
[    0.170008] CPU1: Booted secondary processor [410fd042]
[    0.197980] Detected VIPT I-cache on CPU2
[    0.197999] GICv3: CPU2: found redistributor 2 region 0:0x0000000051b40000
[    0.198022] CPU2: Booted secondary processor [410fd042]
[    0.226049] Detected VIPT I-cache on CPU3
[    0.226070] GICv3: CPU3: found redistributor 3 region 0:0x0000000051b60000
[    0.226090] CPU3: Booted secondary processor [410fd042]
[    0.226166] smp: Brought up 1 node, 4 CPUs
[    0.278158] SMP: Total of 4 processors activated.
[    0.282840] CPU features: detected feature: GIC system register CPU interface
[    0.289976] CPU features: detected feature: 32-bit EL0 Support
[    0.295796] CPU features: detected feature: Kernel page table isolation (KPTI)
[    0.307678] CPU: All CPU(s) started at EL2
[    0.311446] alternatives: patching kernel code
[    0.316215] CPU3: update max cpu_capacity 1024
[    0.320936] devtmpfs: initialized
[    0.328094] CPU3: update max cpu_capacity 1024
[    0.341439] Registered cp15_barrier emulation handler
[    0.346172] Registered setend emulation handler
[    0.351059] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.360516] futex hash table entries: 1024 (order: 5, 131072 bytes)
[    0.392819] pinctrl core: initialized pinctrl subsystem
[    0.400165] DMI not present or invalid.
[    0.404082] NET: Registered protocol family 16
[    0.409680] schedtune: configured to support 5 boost groups
[    0.417559] cpuidle: using governor menu
[    0.423837] vdso: 2 pages (1 code @ ffff000009007000, 1 data @ ffff000009c44000)
[    0.430937] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.444805] DMA: preallocated 256 KiB pool for atomic allocations
[    0.451711] Serial: AMBA PL011 UART driver
[    0.455886] imx rpmsg driver is registered.
[    0.462770] MU and Power domains initialized
[    0.466730] ***** imx8qxp_clocks_init *****
[    0.545309] imx8qxp-pinctrl iomuxc: initialized IMX pinctrl driver
[    0.590056] mxs_phy 5b100000.usbphy: 5b100000.usbphy supply phy-3p0 not found, using dummy regulator
[    0.612289] MU is ready for cross core communication!
[    0.617263] imx-rpmsg 90000000.rpmsg: assigned reserved memory node rpmsg_dma@0x90400000
[    0.625568] virtio_rpmsg_bus virtio0: rpmsg host is online
[    0.628139] virtio_rpmsg_bus virtio0: creating channel rpmsg-vehicle-channel addr 0x1
[    0.638825] virtio_rpmsg_bus virtio0: creating channel rpmsg-i2c-channel addr 0x2
[    0.646487] virtio_rpmsg_bus virtio1: rpmsg host is online
[    0.675866] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[    0.714699] ACPI: Interpreter disabled.
[    0.732620] vgaarb: loaded
[    0.735671] SCSI subsystem initialized
[    0.740101] usbcore: registered new interface driver usbfs
[    0.745387] usbcore: registered new interface driver hub
[    0.750691] usbcore: registered new device driver usb
[    0.756371] usb_phy_generic usbphynop1: usbphynop1 supply vcc not found, using dummy regulator
[    0.769024] i2c i2c-16: LPI2C adapter registered
[    0.776450] i2c i2c-17: LPI2C adapter registered
[    0.783147] i2c i2c-18: LPI2C adapter registered
[    0.796527] i2c-rpmsg virtio0.rpmsg-i2c-channel.-1.2: new channel: 0x400 -> 0x2!
[    0.804383] imx_rpmsg_i2c i2c-rpbus-1: add I2C adapter i2c-rpmsg-adapter successfully
[    0.812649] pca953x 5-0020: 5-0020 supply vcc not found, using dummy regulator
[    0.823905] imx_rpmsg_i2c i2c-rpbus-5: add I2C adapter i2c-rpmsg-adapter successfully
[    0.832658] max732x 12-0068: failed reading
[    0.836536] max732x: probe of 12-0068 failed with error -1
[    0.842025] imx_rpmsg_i2c i2c-rpbus-12: add I2C adapter i2c-rpmsg-adapter successfully
[    0.850953] imx_rpmsg_i2c i2c-rpbus-14: add I2C adapter i2c-rpmsg-adapter successfully
[    0.859385] pca953x 15-001a: 15-001a supply vcc not found, using dummy regulator
[    0.872299] pca953x 15-001d: 15-001d supply vcc not found, using dummy regulator
[    0.884911] imx_rpmsg_i2c i2c-rpbus-15: add I2C adapter i2c-rpmsg-adapter successfully
[    0.892824] media: Linux media interface: v0.10
[    0.897116] Linux video capture interface: v2.00
[    0.901932] pps_core: LinuxPPS API ver. 1 registered
[    0.906580] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.915765] PTP clock support registered
[    0.920968] EDAC MC: Ver: 3.0.0
[    0.924410] dmi: Firmware registration failed.
[    0.929494] clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
[    0.939907] Advanced Linux Sound Architecture Driver Initialized.
[    0.946752] Bluetooth: Core ver 2.22
[    0.950098] NET: Registered protocol family 31
[    0.954428] Bluetooth: HCI device and connection manager initialized
[    0.960773] Bluetooth: HCI socket layer initialized
[    0.965634] Bluetooth: L2CAP socket layer initialized
[    0.970697] Bluetooth: SCO socket layer initialized
[    0.978035] clocksource: Switched to clocksource arch_sys_counter
[    1.041980] VFS: Disk quotas dquot_6.6.0
[    1.045665] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    1.052762] pnp: PnP ACPI: disabled
[    1.067638] NET: Registered protocol family 2
[    1.072421] TCP established hash table entries: 32768 (order: 6, 262144 bytes)
[    1.079756] TCP bind hash table entries: 32768 (order: 7, 524288 bytes)
[    1.086579] TCP: Hash tables configured (established 32768 bind 32768)
[    1.092945] UDP hash table entries: 2048 (order: 4, 65536 bytes)
[    1.098864] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes)
[    1.105425] NET: Registered protocol family 1
[    1.111927] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[    1.120399] kvm [1]: 8-bit VMID
[    1.124547] kvm [1]: GICv3: no GICV resource entry
[    1.129005] kvm [1]: disabling GICv2 emulation
[    1.133453] kvm [1]: GIC system register CPU interface enabled
[    1.139352] kvm [1]: vgic interrupt IRQ1
[    1.143275] kvm [1]: Hyp mode initialized successfully
[    1.152261] audit: initializing netlink subsys (disabled)
[    1.157465] audit: type=2000 audit(0.968:1): state=initialized audit_enabled=0 res=1
[    1.158271] workingset: timestamp_bits=44 max_order=20 bucket_order=0
[    1.182858] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    1.188646] Registering sdcardfs 0.1
[    1.192319] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[    1.198982] fuse init (API version 7.26)
[    1.203073] 9p: Installing v9fs 9p2000 file system support
[    1.213347] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 242)
[    1.220433] io scheduler noop registered
[    1.224556] io scheduler cfq registered (default)
[    1.229024] io scheduler mq-deadline registered
[    1.233546] io scheduler kyber registered
[    1.274284] pwm-backlight lvds_backlight@0: lvds_backlight@0 supply power not found, using dummy regulator
[    1.285523] pwm-backlight lvds_backlight@1: lvds_backlight@1 supply power not found, using dummy regulator
[    1.309583] mxs-dma 5b810000.dma-apbh: initialized
[    1.317491] Bus freq driver module loaded
[    1.330017] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[    1.340992] SuperH (H)SCI(F) driver initialized
[    1.347068] msm_serial: driver initialized
[    1.352628] 5a060000.serial: ttyLP0 at MMIO 0x5a060010 (irq = 49, base_baud = 5000000) is a FSL_LPUAR[    1.363813] console [ttyLP0] enabled
[    1.363813] console [ttyLP0] enabled
[    1.370804] bootconsole [lpuart32] disabled
[    1.370804] bootconsole [lpuart32] disabled
[    1.380060] fsl-lpuart 5a060000.serial: NO DMA tx channel, run at cpu mode
[    1.386957] fsl-lpuart 5a060000.serial: NO DMA rx channel, run at cpu mode
[    1.394845] 5a070000.serial: ttyLP1 at MMIO 0x5a070010 (irq = 50, base_baud = 5000000) is a FSL_LPUART
[    1.406099] 5a080000.serial: ttyLP2 at MMIO 0x5a080010 (irq = 51, base_baud = 5000000) is a FSL_LPUART
[    1.451024] imx8-dpr-channel 560d0000.dpr-channel: Linked as a consumer to 56040000.prg
[    1.459965] imx8-dpr-channel 560e0000.dpr-channel: Linked as a consumer to 56050000.prg
[    1.468027] imx8-dpr-channel 560e0000.dpr-channel: Linked as a consumer to 56040000.prg
[    1.476964] imx8-dpr-channel 560f0000.dpr-channel: Linked as a consumer to 56060000.prg
[    1.487950] imx8-dpr-channel 56100000.dpr-channel: Linked as a consumer to 56070000.prg
[    1.496009] imx8-dpr-channel 56100000.dpr-channel: Linked as a consumer to 56080000.prg
[    1.506915] imx8-dpr-channel 56110000.dpr-channel: Linked as a consumer to 56090000.prg
[    1.514976] imx8-dpr-channel 56110000.dpr-channel: Linked as a consumer to 560a0000.prg
[    1.525897] imx8-dpr-channel 56120000.dpr-channel: Linked as a consumer to 560b0000.prg
[    1.533955] imx8-dpr-channel 56120000.dpr-channel: Linked as a consumer to 560c0000.prg
[    1.546096] dpu-core 56180000.dpu: Linked as a consumer to 56100000.dpr-channel
[    1.553489] dpu-core 56180000.dpu: Linked as a consumer to 56110000.dpr-channel
[    1.560844] dpu-core 56180000.dpu: Linked as a consumer to 560f0000.dpr-channel
[    1.568235] dpu-core 56180000.dpu: Linked as a consumer to 56120000.dpr-channel
[    1.575582] dpu-core 56180000.dpu: Linked as a consumer to 56020000.pixel-combiner
[    1.584529] dpu-core 56180000.dpu: driver probed
[    1.594255] adv7511 17-003d: 17-003d supply avdd not found, using dummy regulator
[    1.601833] adv7511 17-003d: 17-003d supply dvdd not found, using dummy regulator
[    1.609367] adv7511 17-003d: 17-003d supply pvdd not found, using dummy regulator
[    1.616903] adv7511 17-003d: 17-003d supply a2vdd not found, using dummy regulator
[    1.624541] adv7511 17-003d: 17-003d supply v3p3 not found, using dummy regulator
[    1.632083] adv7511 17-003d: 17-003d supply v1p2 not found, using dummy regulator
[    1.640217] adv7511 17-003d: Probe failed. Remote port '/mipi_dsi_bridge@56228000' disabled
[    1.648937] adv7511 18-003d: 18-003d supply avdd not found, using dummy regulator
[    1.656593] adv7511 18-003d: 18-003d supply dvdd not found, using dummy regulator
[    1.664146] adv7511 18-003d: 18-003d supply pvdd not found, using dummy regulator
[    1.671678] adv7511 18-003d: 18-003d supply a2vdd not found, using dummy regulator
[    1.679314] adv7511 18-003d: 18-003d supply v3p3 not found, using dummy regulator
[    1.686847] adv7511 18-003d: 18-003d supply v1p2 not found, using dummy regulator
[    1.694974] adv7511 18-003d: Probe failed. Remote port '/mipi_dsi_bridge@56248000' disabled
[    1.756887] it6263 17-004c: Probe failed. Remote port '/ldb@562210e0/lvds-channel@0' disabled
[    1.821849] it6263 18-004c: Probe failed. Remote port '/ldb@562410e0/lvds-channel@0' disabled
[    1.838144] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[    1.844781] [drm] No driver support for vblank timestamp query.
[    1.850794] dpu-core 56180000.dpu: Linked as a consumer to 560d0000.dpr-channel
[    1.858153] dpu-core 56180000.dpu: Linked as a consumer to 560e0000.dpr-channel
[    1.865509] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[    1.873952] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[    1.881472] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[    1.888855] nwl_dsi-imx mipi_dsi@56228000: No bridge found, skipping encoder creation
[    1.896723] imx-drm display-subsystem: bound mipi_dsi@56228000 (ops imx_nwl_dsi_component_ops)
[    1.905435] nwl_dsi-imx mipi_dsi@56248000: No bridge found, skipping encoder creation
[    1.913297] imx-drm display-subsystem: bound mipi_dsi@56248000 (ops imx_nwl_dsi_component_ops)
[    1.921950] [drm] Cannot find any crtc or sizes
[    1.927463] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 0
[    1.953243] brd: module loaded
[    1.963465] loop: module loaded
[    1.967395] zram: Added device: zram0
[    1.972371] input: fxos8700 as /devices/platform/i2c-rpbus-14/i2c-14/14-001e/input/input0
[    1.982768] fxos8700 device driver probe successfully
[    1.983857] input: fxas2100x as /devices/platform/i2c-rpbus-14/i2c-14/14-0021/input/input1
[    1.997947] fxas2100x 14-0021: fxas2100x device driver probe successfully
[    2.012853] slram: not enough parameters.
[    2.024056] libphy: Fixed MDIO Bus: probed
[    2.029263] NXP PHY: loading NXP PHY driver: [autonomous mode]
[    2.035583] tun: Universal TUN/TAP device driver, 1.6
[    2.040974] CAN device driver interface
[    2.049540] fec 5b040000.ethernet: 5b040000.ethernet supply phy not found, using dummy regulator
[    2.059306] pps pps0: new PPS source ptp0
[    2.070199] libphy: fec_enet_mii_bus: probed
[    2.075637] fec 5b040000.ethernet eth0: registered PHC device 0
[    2.083178] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
[    2.089033] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[    2.095101] igb: Intel(R) Gigabit Ethernet Network Driver - version 5.4.0-k
[    2.102076] igb: Copyright (c) 2007-2014 Intel Corporation.
[    2.107764] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k
[    2.115611] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[    2.122753] sky2: driver version 1.30
[    2.127564] PPP generic driver version 2.4.2
[    2.132153] PPP BSD Compression module registered
[    2.136879] PPP Deflate Compression module registered
[    2.141970] PPP MPPE Compression module registered
[    2.146897] usbcore: registered new interface driver asix
[    2.152456] usbcore: registered new interface driver ax88179_178a
[    2.158677] usbcore: registered new interface driver cdc_ether
[    2.164617] usbcore: registered new interface driver net1080
[    2.170399] usbcore: registered new interface driver cdc_subset
[    2.176432] usbcore: registered new interface driver zaurus
[    2.182220] usbcore: registered new interface driver cdc_ncm
[    2.194188] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    2.200756] ehci-pci: EHCI PCI platform driver
[    2.205368] ehci-platform: EHCI generic platform driver
[    2.211161] ehci-orion: EHCI orion driver
[    2.215558] ehci-exynos: EHCI EXYNOS driver
[    2.220109] ehci-msm: Qualcomm On-Chip EHCI Host Controller
[    2.226004] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[    2.232229] ohci-pci: OHCI PCI platform driver
[    2.236835] ohci-platform: OHCI generic platform driver
[    2.242471] ohci-exynos: OHCI EXYNOS driver
[    2.248365] usbcore: registered new interface driver usb-storage
[    2.254513] usbcore: registered new interface driver usb_ehset_test
[    2.263540] usbmisc_imx 5b0d0200.usbmisc: 5b0d0200.usbmisc supply vbus-wakeup not found, using dummy regulator
[    2.279922] input: sc-powerkey as /devices/platform/sc-powerkey/input/input2
[    2.287582] usbcore: registered new interface driver xpad
[    2.293146] usbcore: registered new interface driver usb_acecad
[    2.299186] usbcore: registered new interface driver aiptek
[    2.304886] usbcore: registered new interface driver gtco
[    2.310401] usbcore: registered new interface driver hanwang
[    2.316183] usbcore: registered new interface driver kbtab
[    2.323581] read mpl3115 chip id 0xc4
[    2.327476] input: mpl3115 as /devices/virtual/input/input3
[    2.333984] mpl3115 device driver probe successfully
[    2.334373] isl29023 15-0044: 15-0044 supply vdd not found, using dummy regulator
[    2.354567] input: isl29023 light sensor as /devices/virtual/input/input4
[    2.361779] isl29023 15-0044: driver version 1.0 enabled
[    2.369889] imx_sc_rtc rtc: rtc core: registered rtc as rtc0
[    2.376391] i2c /dev entries driver
[    2.390469] mxc-mipi-csi2 58227000.csi: mipi_csi2_probe
[    2.416724] mxc-parallel-csi 58261000.pcsi: mxc_parallel_csi_probe probe successfully
[    2.426138] ov5640_v3 5-003c: 5-003c supply DOVDD not found, using dummy regulator
[    2.433809] ov5640_v3 5-003c: 5-003c supply DVDD not found, using dummy regulator
[    2.441365] ov5640_v3 5-003c: 5-003c supply AVDD not found, using dummy regulator
[    2.502170] ov5640_read_reg:write reg error:reg=300a
[    2.507185] camera ov5640 is not found
[    2.513002] ov5640_mipi_v3 16-003c: 16-003c supply DOVDD not found, using dummy regulator
[    2.521254] ov5640_mipi_v3 16-003c: 16-003c supply DVDD not found, using dummy regulator
[    2.529410] ov5640_mipi_v3 16-003c: 16-003c supply AVDD not found, using dummy regulator
[    2.570181] ov5640_mipi_v3 16-003c: Read reg error: reg=300a
[    2.575850] camera ov5640 is not found
[    2.580950] mx8-img-md: Registered mxc_isi.0.capture as /dev/video0
[    2.587636] mx8-img-md: Registered mxc_isi.2.capture as /dev/video1
[    2.594083] mxc-isi 58120000.isi: register m2m device success
[    2.600181] mxc-isi 58100000.isi: mxc_md_unregister_all unregister ISI channel[0]
[    2.607827] mxc-isi 58120000.isi: mxc_md_unregister_all unregister ISI channel[2]
[    2.617293] mxc-jpeg 58400000.jpegdec: decoder device registered as /dev/video0 (81,0)
[    2.626877] mxc-jpeg 58450000.jpegenc: encoder device registered as /dev/video1 (81,1)
[    2.635694] usbcore: registered new interface driver uvcvideo
[    2.641474] USB Video Class driver (1.1.1)
[    2.647315] __power_supply_register: Expected proper parent device for 'battery'
[    2.654977] (NULL device *): hwmon_device_register() is deprecated. Please convert the driver to use hwmon_device_register_with_info().
[    2.667266] __power_supply_register: Expected proper parent device for 'usb'
[    2.681412] device-mapper: uevent: version 1.0.3
[    2.686385] device-mapper: ioctl: 4.37.0-ioctl (2017-09-20) initialised: dm-devel@redhat.com
[    2.695097] Bluetooth: HCI UART driver ver 2.3
[    2.699559] Bluetooth: HCI UART protocol H4 registered
[    2.704719] Bluetooth: HCI UART protocol BCSP registered
[    2.710046] Bluetooth: HCI UART protocol ATH3K registered
[    2.715462] Bluetooth: HCI UART protocol Three-wire (H5) registered
[    2.722094] Bluetooth: HCI UART protocol Broadcom registered
[    2.727770] Bluetooth: HCI UART protocol QCA registered
[    2.733762] bt power gpio is:201
[    2.738334] rfkill: BT RF going to : on
[    2.742045] mxc_bt_rfkill driver success loaded
[    2.742181] mxc_bt_rfkill_reset
[    2.748915] sdhci: Secure Digital Host Controller Interface driver
[    2.756051] sdhci: Copyright(c) Pierre Ossman
[    2.761154] Synopsys Designware Multimedia Card Interface Driver
[    2.769940] sdhci-pltfm: SDHCI platform and OF driver helper
[    2.777939] mmc0: CQHCI version 5.10
[    2.826093] mmc0: SDHCI controller on 5b010000.usdhc [5b010000.usdhc] using ADMA
[    2.838630] mmc1: CQHCI version 5.10
[    2.902047] ##### wifi mmc wl-en ##########
[    2.906300] sdhci-esdhc-imx 5b020000.usdhc: assigned as wifi host
[    2.936948] mmc0: new HS400 MMC card at address 0001
[    2.942700] mmcblk0: mmc0:0001 R1J57L 29.1 GiB
[    2.947680] mmcblk0boot0: mmc0:0001 R1J57L partition 1 8.00 MiB
[    2.954051] mmcblk0boot1: mmc0:0001 R1J57L partition 2 8.00 MiB
[    2.960400] mmcblk0rpmb: mmc0:0001 R1J57L partition 3 4.00 MiB
[    2.962090] mmc1: SDHCI controller on 5b020000.usdhc [5b020000.usdhc] using ADMA
[    2.973188] Alternate GPT is invalid, using primary GPT.
[    2.979052]  mmcblk0: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13 p14 p15
[    2.987459] Galcore version 6.2.4.190076
[    3.009913] random: fast init done
[    3.014880] mmc1: queuing unknown CIS tuple 0x01 (3 bytes)
[    3.028323] mmc1: queuing unknown CIS tuple 0x1a (5 bytes)
[    3.037365] mmc1: queuing unknown CIS tuple 0x1b (8 bytes)
[    3.043570] mmc1: queuing unknown CIS tuple 0x14 (0 bytes)
[    3.055725] mmc1: queuing unknown CIS tuple 0x80 (1 bytes)
[    3.061307] mmc1: queuing unknown CIS tuple 0x81 (1 bytes)
[    3.066870] mmc1: queuing unknown CIS tuple 0x82 (1 bytes)
[    3.072401] mmc1: new high speed SDIO card at address 0001
[    3.114846] [drm] Initialized vivante 1.0.0 20170808 for 80000000.imx8_gpu_ss on minor 1
[    3.152156] ledtrig-cpu: registered to indicate activity on CPUs
[    3.161360] hidraw: raw HID events driver (C) Jiri Kosina
[    3.169792] usbcore: registered new interface driver usbhid
[    3.175404] usbhid: USB HID core driver
[    3.215928] ashmem: initialized
[    3.226840] usbcore: registered new interface driver snd-usb-audio
[    3.254245] cs42xx8 5-0048: found device, revision 4
[    3.260867] wm8960 5-001a: wm8960_i2c_probe(), quick probe 0
[    3.270078] ***** imx8qm_acm_init *****
[    3.307591] imx-cs42888 sound-cs42888: cs42888 <-> 59010000.esai mapping ok
[    3.317718] imx-cs42888 sound-cs42888: snd-soc-dummy-dai <-> 59000000.asrc mapping ok
[    3.325721] imx-cs42888 sound-cs42888: cs42888 <-> 59010000.esai mapping ok
[    3.332796] imx-cs42888 sound-cs42888: ASoC: no DMI vendor name!
[    3.341623] imx-wm8960 sound: wm8960-hifi <-> 59050000.sai mapping ok
[    3.348137] imx-wm8960 sound: ASoC: no source widget found for ASRC-Playback
[    3.355237] imx-wm8960 sound: ASoC: Failed to add route ASRC-Playback -> direct -> CPU-Playback
[    3.363972] imx-wm8960 sound: ASoC: no sink widget found for ASRC-Capture
[    3.370796] imx-wm8960 sound: ASoC: Failed to add route CPU-Capture -> direct -> ASRC-Capture
[    3.379372] imx-wm8960 sound: ASoC: no DMI vendor name!
[    3.497368] imx-xtor sound-xtor: snd-soc-dummy-dai <-> 59040000.sai mapping ok
[    3.504637] imx-xtor sound-xtor: ASoC: no sink widget found for Playback
[    3.511365] imx-xtor sound-xtor: ASoC: Failed to add route CPU-Playback -> direct -> Playback
[    3.519906] imx-xtor sound-xtor: ASoC: no source widget found for Capture
[    3.526716] imx-xtor sound-xtor: ASoC: Failed to add route Capture -> direct -> CPU-Capture
[    3.535082] imx-xtor sound-xtor: ASoC: no DMI vendor name!
[    3.543338] imx-amix sound-amix-sai: DAI FE name:HiFi-AMIX-FE-sai@59820000
[    3.550373] imx-amix sound-amix-sai: DAI FE name:HiFi-AMIX-FE-sai@59830000
[    3.557803] imx-amix sound-amix-sai: snd-soc-dummy-dai <-> 59820000.sai mapping ok
[    3.565481] imx-amix sound-amix-sai: snd-soc-dummy-dai <-> 59830000.sai mapping ok
[    3.573117] imx-amix sound-amix-sai: snd-soc-dummy-dai <-> amix-0 mapping ok
[    3.580229] imx-amix sound-amix-sai: snd-soc-dummy-dai <-> amix-1 mapping ok
[    3.587315] imx-amix sound-amix-sai: ASoC: no DMI vendor name!
[    3.596256] NET: Registered protocol family 26
[    3.600738] u32 classifier
[    3.603457]     Actions configured
[    3.606884] Netfilter messages via NETLINK v0.30.
[    3.611870] nf_conntrack version 0.5.0 (16384 buckets, 65536 max)
[    3.618187] ctnetlink v0.93: registering with nfnetlink.
[    3.623953] xt_time: kernel timezone is -0000
[    3.628437] IPv4 over IPsec tunneling driver
[    3.633221] ip_tables: (C) 2000-2006 Netfilter Core Team
[    3.639047] arp_tables: arp_tables: (C) 2002 David S. Miller
[    3.644829] Initializing XFRM netlink socket
[    3.649572] NET: Registered protocol family 10
[    3.655072] Segment Routing with IPv6
[    3.658837] mip6: Mobile IPv6
[    3.661819] ip6_tables: (C) 2000-2006 Netfilter Core Team
[    3.668100] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[    3.674941] NET: Registered protocol family 17
[    3.679432] NET: Registered protocol family 15
[    3.683888] can: controller area network core (rev 20170425 abi 9)
[    3.690143] NET: Registered protocol family 29
[    3.694610] can: raw protocol (rev 20170425)
[    3.698891] can: broadcast manager protocol (rev 20170425 t)
[    3.704572] can: netlink gateway (rev 20170425) max_hops=1
[    3.710289] Bluetooth: RFCOMM TTY layer initialized
[    3.715192] Bluetooth: RFCOMM socket layer initialized
[    3.720374] Bluetooth: RFCOMM ver 1.11
[    3.724169] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[    3.729510] Bluetooth: BNEP filters: protocol multicast
[    3.734763] Bluetooth: BNEP socket layer initialized
[    3.739767] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[    3.745704] Bluetooth: HIDP socket layer initialized
[    3.750680] lib80211: common routines for IEEE802.11 drivers
[    3.756761] 9pnet: Installing 9P2000 support
[    3.763045] registered taskstats version 1
[    3.786122] imx8_cpufreq_init: cluster 0 running at freq 1200 MHz, suspend freq 1200 MHz
[    3.805562] OF: PCI: host bridge /pcie@0x5f010000 ranges:
[    3.810990] OF: PCI:   No bus range found for /pcie@0x5f010000, using [bus 00-ff]
[    3.818506] OF: PCI:    IO 0x7ff80000..0x7ff8ffff -> 0x00000000
[    3.824450] OF: PCI:   MEM 0x70000000..0x7fefffff -> 0x70000000
[    3.831692] imx6q-pcie 5f010000.pcie: pcie phy pll is locked.
[    4.082748] imx6q-pcie 5f010000.pcie: phy link never came up
[    4.088436] imx6q-pcie 5f010000.pcie: failed to initialize host
[    4.094375] imx6q-pcie 5f010000.pcie: unable to add pcie port.
[    4.100534] imx6q-pcie: probe of 5f010000.pcie failed with error -110
[    4.113216] Can't support > 32 bit dma.
[    4.117114]  xhci-cdns3: xHCI Host Controller
[    4.121508]  xhci-cdns3: new USB bus registered, assigned bus number 1
[    4.174839]  xhci-cdns3: hcc params 0x200073c8 hci version 0x100 quirks 0xffffffffa0010010
[    4.183320] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[    4.190145] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    4.197384] usb usb1: Product: xHCI Host Controller
[    4.202273] usb usb1: Manufacturer: Linux 4.14.98 xhci-hcd
[    4.207772] usb usb1: SerialNumber: xhci-cdns3
[    4.212828] hub 1-0:1.0: USB hub found
[    4.216623] hub 1-0:1.0: 1 port detected
[    4.220864]  xhci-cdns3: xHCI Host Controller
[    4.225249]  xhci-cdns3: new USB bus registered, assigned bus number 2
[    4.231811]  xhci-cdns3: Host supports USB 3.0  SuperSpeed
[    4.237412] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[    4.245656] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003
[    4.252487] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    4.259730] usb usb2: Product: xHCI Host Controller
[    4.264623] usb usb2: Manufacturer: Linux 4.14.98 xhci-hcd
[    4.270127] usb usb2: SerialNumber: xhci-cdns3
[    4.275047] hub 2-0:1.0: USB hub found
[    4.278840] hub 2-0:1.0: 1 port detected
[    4.300294] imx_sc_rtc rtc: setting system clock to 2020-04-17 07:57:00 UTC (1587110220)
[    4.311103] usb_otg1_vbus: disabling
[    4.314705] ALSA device list:
[    4.317674]   #0: cs42888-audio
[    4.320827]   #1: wm8960-audio
[    4.323896]   #2: xtor-audio
[    4.326787]   #3: amix-audio-sai
[    4.332439] device-mapper: init: attempting early device configuration.
[    4.339825] device-mapper: init: adding target '0 3611944 verity 1 PARTUUID=628e7189-62e6-406e-98b8-41b6a8254a55 PARTUUID=628e7189-62e6-406e-98b8-41b6a8254a55 4096 4096 451493 451493 sha1 2e59d456cdd5c07961943800072d5b4bd7f5a0e5 9c9f947fb565b400d48b47df9b93b2b6099625a7 10 restart_on_corruption ignore_zero_blocks use_fec_from_device PARTUUID=628e7189-62e6-406e-98b8-41b6a8254a55 fec_roots 2 fec_blocks 455050 fec_start 455050'
[    4.386606] device-mapper: init: dm-0 is ready
[    4.402215] EXT4-fs (dm-0): mounted filesystem without journal. Opts: (null)
[    4.409341] VFS: Mounted root (ext4 filesystem) readonly on device 252:0.
[    4.418884] devtmpfs: mounted
[    4.423770] Freeing unused kernel memory: 5504K
[    4.460574] init: init first stage started!
[    4.465602] init: Using Android DT directory /proc/device-tree/firmware/android/
[    4.475912] init: [libfs_mgr]fs_mgr_read_fstab_default(): failed to find device default fstab
[    4.525892] init: [libfs_mgr]Returning avb_handle with status: 0
[    4.537443] init: [libfs_mgr]Loading verity table: '1 /dev/block/platform/5b010000.usdhc/by-name/vendor_a /dev/block/platform/5b010000.usdhc/by-name/vendor_a 4096 4096 64481 64481 sha1 f37f1e377f982513f2adfe45f066b2ab981df4d9 4f0a8ca37bbe42db781790e0b43d06043962d9d2 10 use_fec_from_device /dev/block/platform/5b010000.usdhc/by-name/vendor_a fec_roots 2 fec_blocks 64990 fec_start 64990 restart_on_corruption ignore_zero_blocks'
[    4.592297] EXT4-fs (dm-1): mounted filesystem without journal. Opts: barrier=1,inode_readahead_blks=8
[    4.601797] init: [libfs_mgr]__mount(source=/dev/block/dm-1,target=/vendor,type=ext4)=0: Success
[    4.610842] init: Skipped setting INIT_AVB_VERSION (not in recovery mode)
[    4.617923] init: Loading SELinux policy
[    4.657140] SELinux:  Class process2 not defined in policy.
[    4.663434] SELinux:  Class infiniband_pkey not defined in policy.
[    4.669630] SELinux:  Class infiniband_endport not defined in policy.
[    4.676087] SELinux: the above unknown classes and permissions will be denied
[    4.683267] SELinux:  policy capability network_peer_controls=1
[    4.689200] SELinux:  policy capability open_perms=1
[    4.694297] SELinux:  policy capability extended_socket_class=1
[    4.700238] SELinux:  policy capability always_check_network=0
[    4.706077] SELinux:  policy capability cgroup_seclabel=0
[    4.711488] SELinux:  policy capability nnp_nosuid_transition=0
[    4.864997] audit: type=1403 audit(1587110221.060:2): policy loaded auid=4294967295 ses=4294967295
[    4.865210] selinux: SELinux: Loaded policy from /vendor/etc/selinux/precompiled_sepolicy
[    4.865210]
[    4.884328] audit: type=1404 audit(1587110221.080:3): enforcing=1 old_enforcing=0 auid=4294967295 ses=4294967295
[    4.916093] selinux: SELinux: Loaded file_contexts
[    4.916093]
[    4.928237] init: init second stage started!
[    4.963413] init: Using Android DT directory /proc/device-tree/firmware/android/
[    4.977835] selinux: SELinux: Loaded file_contexts
[    4.977835]
[    4.984239] init: Running restorecon...
[    5.000509] init: waitid failed: No child processes
[    5.014726] init: Couldn't load property file '/odm/default.prop': open() failed: No such file or directory: No such file or directory
[    5.028924] init: Created socket '/dev/socket/property_service', mode 666, user 0, group 0
[    5.038267] init: Forked subcontext for 'u:r:vendor_init:s0' with pid 2458
[    5.046014] init: Forked subcontext for 'u:r:vendor_init:s0' with pid 2459
[    5.053234] init: Parsing file /init.rc...
[    5.122180] audit: type=1400 audit(1587110221.320:4): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
[    5.129443] ueventd: ueventd started!
[    5.139790] audit: type=1400 audit(1587110221.320:5): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
[    5.139798] audit: type=1400 audit(1587110221.320:6): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
[    5.139807] audit: type=1400 audit(1587110221.320:7): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
[    5.148896] selinux: SELinux: Loaded file_contexts
[    5.148896]
[    5.161055] audit: type=1400 audit(1587110221.324:8): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
[    5.161061] audit: type=1400 audit(1587110221.324:9): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
[    5.161068] audit: type=1400 audit(1587110221.324:10): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
[    5.255749] ueventd: Parsing file /ueventd.rc...
[    5.263301] ueventd: Parsing file /vendor/ueventd.rc...
[    5.269733] ueventd: Parsing file /odm/ueventd.rc...
[    5.274856] ueventd: Unable to read config file '/odm/ueventd.rc': open() failed: No such file or directory
[    5.284933] ueventd: Parsing file /ueventd.freescale.rc...
[    5.290571] ueventd: Unable to read config file '/ueventd.freescale.rc': open() failed: No such file or directory
[    5.472271] wlan: loading out-of-tree module taints kernel.
[    5.555239] ueventd: Coldboot took 0.251 seconds
[    5.591571] Registered swp emulation handler
[    5.603683] watchdogd: watchdogd started (interval 10, margin 20)!
[    5.631638] EXT4-fs (mmcblk0p12): Ignoring removed nomblk_io_submit option
[    5.649065] EXT4-fs (mmcblk0p12): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic
[    5.703878] zram0: detected capacity change from 0 to 314572800
[    5.749003] logd.auditd: start
[    5.752275] logd.klogd: 5566215625
[    5.758746] mkswap: Swapspace size: 307196k, UUID=a7be6290-e5e5-4ee3-a4fd-9b8b79beab1d
[    5.768608] Adding 307196k swap on /dev/block/zram0.  Priority:-2 extents:1 across:307196k SS
[    5.868986] wlan: loading driver v4.0.11.213V
[    5.875776] type=1400 audit(1587110221.976:38): avc: denied { getattr } for pid=2458 comm="init" path="/data/cache" dev="mmcblk0p12" ino=24 scontext=u:r:vendor_init:s0 tcontext=u:object_r:cache_file:s0 tclass=dir permissive=0
[    5.898071] AR6000: hifDeviceInserted, Function: 0x1, Vendor ID: 0x271, Device ID: 0x701, block size: 0x800/0x200
[    5.909212] type=1400 audit(1587110221.976:38): avc: denied { getattr } for pid=2458 comm="init" path="/data/cache" dev="mmcblk0p12" ino=24 scontext=u:r:vendor_init:s0 tcontext=u:object_r:cache_file:s0 tclass=dir permissive=0
[    5.914254] hifDeviceInserted: Dumping clocks (50000000,50000000)
[    5.929346] type=1400 audit(1587110221.980:39): avc: denied { dac_read_search } for pid=1 comm="init" capability=2 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
[    5.935380] HIFDumpCCCR
[    5.935419] 0(43)
[    5.954791] 1(3)
[    5.956838] 2(0)
[    5.958812] 3(0)
[    5.960776] 4(0)
[    5.962848] 5(0)
[    5.964889] 6(0)
[    5.966951] 7(6)
[    5.968968] 8(17)
[    5.970985] 9(0)
[    5.973075] A(10)
[    5.975106] B(0)
[    5.977180] C(0)
[    5.979210] D(0)
[    5.981207] E(0)
[    5.983154] F(0)
[    5.985186] 10(0)
[    5.987208] 11(0)
[    5.989299] 12(1)
[    5.991452] 13(3)
[    5.993580] 14(7)
[    5.995798] 15(37)
[    5.997932] 16(1)
[    6.000099]
[    6.004151] AR6000: Set async interrupt delay clock as 2.
[    6.011692] firmware_path=/vendor/etc/firmware/wlan/qcom_cfg.ini
[    6.025124] R0: wlan: [2712:E :HDD] hdd_apply_cfg_ini: Reg Parameter 5g_rssi_boost_threshold < allowed Minimum [4294967236 < 18446744073709551546]. Enforcing Default= 18446744073709551556
[    6.041942] R0: wlan: [2712:E :HDD] hdd_apply_cfg_ini: Reg Parameter 5g_rssi_penalize_threshold < allowed Minimum [4294967226 < 18446744073709551536]. Enforcing Default= 18446744073709551546
[    6.059131] R0: wlan: [2712:E :HDD] Name = [gEnableHostapdEdcaLocal] Value = [0]
[    6.066675] R0: wlan: [2712:E :HDD] Name = [g_sta_change_cc_via_beacon] Value = [0]
[    6.193883] AR6000: configuration opcode 3 is not used for Linux SDIO stack
[    6.201736] NUM_DEV=1 FWMODE=0x2 FWSUBMODE=0x0 FWBR_BUF 0
[    6.212663] ol_download_firmware: Using 0x1234 for the remainder of init
[    6.219421] firmware_path=/vendor/etc/firmware/otp30.bin
[    6.270177] ol_download_firmware: chip_id:0x5020001 board_id:0x0
[    6.276503] firmware_path=/vendor/etc/firmware/bdwlan30.b00
[    6.282432] firmware_path=/lib/firmware/updates/4.14.98/bdwlan30.b00
[    6.288880] firmware_path=/lib/firmware/updates/bdwlan30.b00
[    6.294797] firmware_path=/lib/firmware/4.14.98/bdwlan30.b00
[    6.300544] firmware_path=/lib/firmware/bdwlan30.b00
[    6.304106] update_verifier: Started with arg 1: nonencrypted
[    6.305857] firmware_path=/system/etc/firmware/bdwlan30.b00
[    6.317011] firmware_path=/vendor/etc/firmware/bdwlan30.b00
[    6.317143] update_verifier: Booting slot 0: isSlotMarkedSuccessful=1
[    6.322824] ar6k_wlan mmc1:0001:1: Falling back to user helper
[    6.329112] update_verifier: Leaving update_verifier.
[    6.336441] ueventd: firmware: loading 'bdwlan30.b00' for '/devices/platform/5b020000.usdhc/mmc_host/mmc1/mmc1:0001/mmc1:0001:1/firmware/bdwlan30.b00'
[    6.382354] rfkill: BT RF going to : off
[    6.414939] logd.daemon: reinit
[    6.428094] Mass Storage Function, version: 2009/09/11
[    6.433487] LUN: removable file: (no medium)
[    6.444756] using random self ethernet address
[    6.449297] using random host ethernet address
[    6.456510] __ol_transfer_bin_file: Failed to get bdwlan30.b00:-11
[    6.456513] file system registered
[    6.466221] __ol_transfer_bin_file: Trying to load default bdwlan30.bin
[    6.473249] firmware_path=/vendor/etc/firmware/bdwlan30.bin
[    6.489796] Board extended Data download address: 0x0
[    6.514246] __ol_transfer_bin_file: Loading setup file qsetup30.bin
[    6.520634] firmware_path=/vendor/etc/firmware/qsetup30.bin
[    6.526694] firmware_path=/lib/firmware/updates/4.14.98/qsetup30.bin
[    6.533206] firmware_path=/lib/firmware/updates/qsetup30.bin
[    6.538989] firmware_path=/lib/firmware/4.14.98/qsetup30.bin
[    6.544760] firmware_path=/lib/firmware/qsetup30.bin
[    6.549831] firmware_path=/system/etc/firmware/qsetup30.bin
[    6.555514] firmware_path=/vendor/etc/firmware/qsetup30.bin
[    6.561262] ar6k_wlan mmc1:0001:1: Falling back to user helper
[    6.570618] __ol_transfer_bin_file: Failed to get qsetup30.bin:-11
[    6.576953] firmware_path=/vendor/etc/firmware/qwlan30.bin
[    6.795903] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[    6.803660] audit_log_lost: 29 callbacks suppressed
[    6.803666] audit: audit_lost=362 audit_rate_limit=5 audit_backlog_limit=64
[    6.840344] audit: rate limit exceeded
[    7.038136] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[    7.129534] AR6000: SDIO bus operation failed! MMC stack returned : -84
[    7.146923] __HIFReadWrite, addr:0X000850, len:00000004, Read , Sync
[    7.158130] Unable to decrement the command credit count register
[    7.179077] BMI : Unable to Send Message to device
mek_8q:/ $ [    7.198081] Unable to write to the device
[    7.217677] __ol_transfer_bin_file, BMI operation failed: 966
[    7.244067] input: FSL_SENS_HUB as /devices/virtual/input/input6
[    7.246321] R0: wlan: [2712:F :HIF]  hdd_wlan_startup failed
[    7.290825] ar6k_wlan: probe of mmc1:0001:1 failed with error -1
[    7.315237] ath_hif_sdio: HIF (Atheros/multi-bss)
[    7.330578] R0: wlan: [2712:E :HDD] hdd_hif_register_driver: 17769: hdd_wlan_startup failed status:-11 jiffies_left:35000
[    7.366122] R0: wlan: [2712:F :HDD] hdd_driver_init: WLAN Driver Initialization failed
[    7.398109] AR6000: Unregistering with the bus driver
[    7.422983] AR6000: Unregistered!
[    7.778563] firmware_path=/vendor/etc/firmware/vpu/vpu_fw_imx8_enc.bin
[    7.837544] firmware_path=/lib/firmware/updates/4.14.98/vpu/vpu_fw_imx8_enc.bin
[    7.860509] firmware_path=/lib/firmware/updates/vpu/vpu_fw_imx8_enc.bin
[    7.870292] firmware_path=/lib/firmware/4.14.98/vpu/vpu_fw_imx8_enc.bin
[    7.886319] firmware_path=/lib/firmware/vpu/vpu_fw_imx8_enc.bin
[    7.898331] firmware_path=/system/etc/firmware/vpu/vpu_fw_imx8_enc.bin
[    7.905514] audit: audit_lost=501 audit_rate_limit=5 audit_backlog_limit=64
[    7.918130] audit: rate limit exceeded
[    7.925780] firmware_path=/vendor/etc/firmware/vpu/vpu_fw_imx8_enc.bin
[    7.956292] vpu-b0-encoder 2d000000.vpu_encoder: Falling back to user helper
[    7.986845] read descriptors
[    7.990297] read strings
[    8.004606] [VPU Encoder]     enable mu for core[0]
[    8.017584] [VPU Encoder]     vpu encoder core[0] firmware version is 1.2.2
[    8.045017] firmware_path=/vendor/etc/firmware/vpu/vpu_fw_imx8_dec.bin
[    8.052439] firmware_path=/lib/firmware/updates/4.14.98/vpu/vpu_fw_imx8_dec.bin
[    8.074133] firmware_path=/lib/firmware/updates/vpu/vpu_fw_imx8_dec.bin
[    8.102147] firmware_path=/lib/firmware/4.14.98/vpu/vpu_fw_imx8_dec.bin
[    8.110418] firmware_path=/lib/firmware/vpu/vpu_fw_imx8_dec.bin
[    8.118289] firmware_path=/system/etc/firmware/vpu/vpu_fw_imx8_dec.bin
[    8.132531] firmware_path=/vendor/etc/firmware/vpu/vpu_fw_imx8_dec.bin
[    8.140459] vpu-b0 2c000000.vpu_decoder: Falling back to user helper
[    8.421690] random: crng init done
[   10.157784] capability: warning: `main' uses 32-bit capabilities (legacy support in use)
[   13.079370] type=1400 audit(1587110225.800:585): avc: denied { dac_read_search } for pid=1 comm="init" capability=2 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0 duplicate messages suppressed
[   13.090135] audit: audit_lost=526 audit_rate_limit=5 audit_backlog_limit=64
[   13.099022] type=1400 audit(1587110229.276:586): avc: denied { dac_read_search } for pid=3167 comm="Binder:3167_1" capability=2 scontext=u:r:installd:s0 tcontext=u:r:installd:s0 tclass=capability permissive=0
[   13.105766] audit: rate limit exceeded
[   13.433593] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[   13.433649] misc FreescaleGyroscope: mma enable setting active
[   13.444459] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[   13.450297] misc FreescaleGyroscope: mma enable setting active
[   13.464071] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[   13.473993] misc FreescaleGyroscope: mma enable setting active
[   13.490767] misc FreescaleGyroscope: mma enable setting active
[   13.500990] misc FreescaleGyroscope: mma enable setting active
[   13.873280] init: processing action (sys.sysctl.extra_free_kbytes=*) from (/init.rc:725)
[   14.126401] type=1400 audit(1587110229.284:591): avc: denied { dac_read_search } for pid=3167 comm="Binder:3167_1" capability=2 scontext=u:r:installd:s0 tcontext=u:r:installd:s0 tclass=capability permissive=0 duplicate messages suppressed
[   14.126686] audit: audit_lost=1758 audit_rate_limit=5 audit_backlog_limit=64
[   14.170096] audit: rate limit exceeded
[   14.186145] type=1400 audit(1587110230.320:1824): avc: denied { dac_read_search } for pid=3167 comm="Binder:3167_2" capability=2 scontext=u:r:installd:s0 tcontext=u:r:installd:s0 tclass=capability permissive=0
[   14.667908] read descriptors
[   14.670897] read strings
[   14.673614] read descriptors
[   14.676627] read strings
[   14.703478] acc_open
[   14.705703] acc_release
[   14.998887] Atheros 8031 ethernet 5b040000.ethernet-1:00: attached PHY driver [Atheros 8031 ethernet] (mii_bus:phy_addr=5b040000.ethernet-1:00, irq=POLL)
[   15.013658] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[   15.044987] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[   15.140390] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[   15.218630] type=1400 audit(1587110230.324:1828): avc: denied { dac_read_search } for pid=3167 comm="Binder:3167_2" capability=2 scontext=u:r:installd:s0 tcontext=u:r:installd:s0 tclass=capability permissive=0 duplicate messages suppressed
[   15.246556] type=1400 audit(1587110231.412:2358): avc: denied { dac_read_search } for pid=3426 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
[   15.248891] sdcardfs version 2.0
[   15.270374] sdcardfs: dev_name -> /data/media
[   15.279212] sdcardfs: options -> fsuid=1023,fsgid=1023,multiuser,derive_gid,default_normal,mask=6,userid=0,gid=1015
[   15.292321] audit: audit_lost=2287 audit_rate_limit=5 audit_backlog_limit=64
[   15.302489] sdcardfs: mnt -> ffff80083a822fe0
[   15.307865] sdcardfs: mounted on top of /data/media type ext4
[   15.313979] audit: rate limit exceeded
[   15.318742] Remount options were mask=23,gid=9997 for vfsmnt ffff80082fb471a0.
[   15.334352] sdcardfs : options - debug:1
[   15.335983] type=1400 audit(1587110231.412:2361): avc: denied { dac_read_search } for pid=3426 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0 duplicate messages suppressed
[   15.338314] sdcardfs : options - gid:9997
[   15.338323] sdcardfs : options - mask:23
[   15.367174] Remount options were mask=7,gid=9997 for vfsmnt ffff80082fb47de0.
[   15.370009] type=1400 audit(1587110231.488:2362): avc: denied { dac_read_search } for pid=3445 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
[   15.374700] sdcardfs : options - debug:1
[   15.396622] sdcardfs : options - gid:9997
[   15.400829] sdcardfs : options - mask:7
[   16.311967] type=1400 audit(1587110231.488:2362): avc: denied { dac_read_search } for pid=3445 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
[   16.339378] type=1400 audit(1587110232.508:2378): avc: denied { dac_read_search } for pid=3625 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
[   16.363515] audit: audit_lost=2302 audit_rate_limit=5 audit_backlog_limit=64
[   16.374832] audit: rate limit exceeded
[   19.735397] misc FreescaleGyroscope: mma enable setting active
[   19.801096] init: Service 'bootanim' (pid 3265) exited with status 0
[   19.843335] init: processing action (sys.boot_completed=1) from (/init.rc:719)
[   19.851798] init: processing action (sys.boot_completed=1) from (/vendor/etc/init/hw/init.freescale.imx8qxp.rc:24)
[   19.876849] init: processing action (sys.boot_completed=1) from (/vendor/etc/init/hw/init.freescale.imx8qxp.rc:30)
[   19.885206] type=1400 audit(1587110232.560:2382): avc: denied { dac_read_search } for pid=3634 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
[   19.896250] audit: audit_lost=2310 audit_rate_limit=5 audit_backlog_limit=64
[   19.905468] init: processing action (sys.boot_completed=1 && sys.logbootcomplete=1) from (/system/etc/init/bootstat.rc:70)
[   19.907751] type=1400 audit(1587110236.080:2391): avc: denied { dac_read_search } for pid=3048 comm="Binder:3048_3" capability=2 scontext=u:r:vold:s0 tcontext=u:r:vold:s0 tclass=capability permissive=0
[   19.912340] audit: rate limit exceeded
[   19.924471] init: starting service 'exec 6 (/system/bin/bootstat --set_system_boot_reason --record_boot_complete --record_boot_reason --record_time_since_factory_reset -l)'...
[   19.963977] init: processing action (sys.boot_completed=1 && sys.wifitracing.started=0) from (/system/etc/init/wifi-events.rc:20)
[   20.051899] init: Command 'mkdir /sys/kernel/debug/tracing/instances/wifi 711' action=sys.boot_completed=1 && sys.wifitracing.started=0 (/system/etc/init/wifi-events.rc:22) took 76ms and succeeded
[   20.073071] selinux: SELinux: Skipping restorecon_recursive(/data/system_ce/0)
[   20.073071]
[   20.106763] init: Async property child exited with status 0
[   21.123885] type=1400 audit(1587110236.084:2395): avc: denied { dac_read_search } for pid=3048 comm="Binder:3048_3" capability=2 scontext=u:r:vold:s0 tcontext=u:r:vold:s0 tclass=capability permissive=0 duplicate messages suppressed
[   21.171649] type=1400 audit(1587110237.320:3620): avc: denied { dac_read_search } for pid=3833 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
[   21.200168] audit: audit_lost=3534 audit_rate_limit=5 audit_backlog_limit=64
[   21.207544] audit: rate limit exceeded
[   21.215950] type=1400 audit(1587110237.320:3623): avc: denied { dac_read_search } for pid=3833 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0 duplicate messages suppressed
[   21.237285] type=1400 audit(1587110237.396:3624): avc: denied { dac_read_search } for pid=3848 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
[   22.277205] type=1400 audit(1587110237.396:3624): avc: denied { dac_read_search } for pid=3848 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
[   22.299586] type=1400 audit(1587110238.472:3644): avc: denied { dac_read_search } for pid=3964 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
[   27.779675] type=1400 audit(1587110238.472:3647): avc: denied { dac_read_search } for pid=3964 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0 duplicate messages suppressed
[   27.800409] type=1400 audit(1587110243.976:3648): avc: denied { dac_read_search } for pid=3994 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
[   27.978909] audit: audit_lost=3553 audit_rate_limit=5 audit_backlog_limit=64
[   27.979547] type=1400 audit(1587110243.980:3651): avc: denied { dac_read_search } for pid=3994 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0 duplicate messages suppressed
[   27.986456] audit: rate limit exceeded
[   28.009261] type=1400 audit(1587110244.172:3652): avc: denied { dac_read_search } for pid=4011 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
[   29.078109] type=1400 audit(1587110244.176:3653): avc: denied { dac_read_search } for pid=4011 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
[   29.096978] type=1400 audit(1587110245.272:3672): avc: denied { dac_read_search } for pid=4119 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
[   29.250176] audit: audit_lost=3571 audit_rate_limit=5 audit_backlog_limit=64
[   29.257541] type=1400 audit(1587110245.276:3675): avc: denied { dac_read_search } for pid=4119 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0 duplicate messages suppressed
[   29.266124] audit: rate limit exceeded
[   29.279229] type=1400 audit(1587110245.444:3676): avc: denied { dac_read_search } for pid=4137 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
[   38.611623] init: Received sys.powerctl='reboot,Received ACTION_REBOOT broadcast' from pid: 3286 (system_server)
[   38.622751] init: Clear action queue and start shutdown trigger
[   38.629373] init: processing action (shutdown_done) from (<Builtin Action>:0)
[   38.638094] init: Reboot start, reason: reboot,Received ACTION_REBOOT broadcast, rebootTarget: Received ACTION_REBOOT broadcast
[   38.674516] init: Shutdown timeout: 6000 ms
[   38.682336] init: starting service 'blank_screen'...
[   38.688681] type=1400 audit(1587110245.444:3676): avc: denied { dac_read_search } for pid=4137 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
[   38.689628] init: terminating init services
[   38.709832] type=1400 audit(1587110254.884:3688): avc: denied { dac_read_search } for pid=1 comm="init" capability=2 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
[   38.710803] init: Sending signal 15 to service 'update_engine' (pid 3184) process group...
[   38.737207] audit: audit_lost=3582 audit_rate_limit=5 audit_backlog_limit=64
[   38.744588] audit: rate limit exceeded
[   38.748863] init: Sending signal 15 to service 'perfprofd' (pid 3179) process group...
[   38.757864] init: Sending signal 15 to service 'gatekeeperd' (pid 3176) process group...
143|mek_8q:/ $ [   38.998781] binder: release 3141:3342 transaction 22632 in, still active
[   39.005591] binder: send failed reply for transaction 22632 to 3286:3350
[   39.423554] android_work: did not send uevent (0 0           (null))
[   39.435928] logd.auditd: 2 output lines suppressed due to ratelimiting
[   39.550849] binder: undelivered TRANSACTION_COMPLETE
[   39.556080] binder: undelivered TRANSACTION_ERROR: 29189
[   39.574814] binder: undelivered transaction 22781, process died.
[   39.580994] binder: undelivered transaction 22782, process died.
[   39.587131] binder: undelivered transaction 22783, process died.
[   39.597117] binder: undelivered transaction 22780, process died.
[   39.880149] kvm: exiting hardware virtualization
[   39.934731] reboot: Restarting system with command 'Received ACTION_REBOOT broadcast'
0 项奖励
3 回复数

3,154 次查看
kevinpwchen
Contributor II

Hi junjie_tan,

I am getting the same problem. Have you solved this issue? If yes, could you share the root cause and solution whit me? Thank you!

Kevin

0 项奖励

3,217 次查看
joanxie
NXP TechSupport
NXP TechSupport

it seems that you have error on PCIe initiation, did you use QCA6174A PCIE wifi and linux 4.14.98 bsp?

0 项奖励

3,217 次查看
junjie_tan
Contributor I

Test procedure: The machine restarts and then insmod wlan.ko has a certain probability of appearing in this failure

0 项奖励