A problem about downloading the image to the i.MX6Q by ourself development

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

A problem about downloading the image to the i.MX6Q by ourself development

773件の閲覧回数
pengxingwei
Contributor III

Dear all,

          I download the android  image to my i,mx6q development board using the MFGtools,but during the process ,it stop at Jumping to OS,such as:

pastedImage_0.png pastedImage_1.png

and the image of jb4.3_1.1.0 is downed from the freescale website.How to solve the problem ? Thanks!

ラベル(2)
0 件の賞賛
6 返答(返信)

573件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi peng

from log: "i.MX6Q-SabreSD and Boot Device :SPI NOR" seems

reason may be that spi-nor boot is not supported for SabreSD,

but supported for Sabre AI boards. One can try to rebuild images

(mfg tools firmware and linux) based on Sabre AI board configuration,

and reuse profile "MX6Q-Sabreauto-SPI_NOR & SD card" in ucl2.xml

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

573件の閲覧回数
pengxingwei
Contributor III

But the MFGTools's  cfg.ini  is:pastedImage_0.png

the Board was made by ourself according to i.MX6Q-SDB of freescale.

0 件の賞賛

573件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

what is the meaning "Boot Device :SPI NOR"  from your log ?

0 件の賞賛

573件の閲覧回数
pengxingwei
Contributor III

For that,I don't kown why the Boot Device is SPI NOR ,but I think it should be:Boot Device: MMC

0 件の賞賛

573件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

I think you can check boot settings for that.

0 件の賞賛

573件の閲覧回数
pengxingwei
Contributor III

Thank you !how to check it ?

0 件の賞賛