Hi Supporter,
We follow 8MMINID4 to design a new HW and replace NAND to eMMC as below.
We can update image successfully by using UUU tool. Please check UUU log and uuu.auto for command list.
After reboot, it will hang up at u-boot and complain "MMC Device 1 not found".
Can you help to check and advise?
boot up log:
U-Boot SPL 2019.04-lf-5.4.y_v2019.04+g48508669 (Dec 02 2020 - 02:47:35 +0000)
power_pca9450_init
DDRINFO: start DRAM init
Training FAILED
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from MMC2
MMC Device 1 not found
spl: could not find mmc device 1. error: -19
SPL: failed to boot from all boot devices
In U-boot prompt, we can found eMMC device at port2.
log:
u-boot=>
u-boot=> mmc list
FSL_SDHC: 2
u-boot=> mmc dev 1
MMC Device 1 not found
no mmc device at slot 1
u-boot=> mmc dev 2
switch to partitions #0, OK
mmc2(part 0) is current device
u-boot=>
Regards,
Kenny
已解决! 转到解答。
In the software the uSDHC3 clock is not initialized in default. We must let CONFIG_SYS_FSL_USDHC_NUM=2 to run the uSDHC3 clock initialization code. How to add you can refer to the thread by my colleague.
In the software the uSDHC3 clock is not initialized in default. We must let CONFIG_SYS_FSL_USDHC_NUM=2 to run the uSDHC3 clock initialization code. How to add you can refer to the thread by my colleague.