4bits bus width emmc prebuild image for sabresd

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

4bits bus width emmc prebuild image for sabresd

1,342件の閲覧回数
xaviercarcelle
Contributor I

hi there,

for production issues, we are looking for a prebuild linux image for 4bits-bus-width emmc used my MfgTool.

This prebuild image is used to be loaded in ocram and then writing uboot in emmc using dd commands.

The available images for sabre-sd and others boards seem to be built for 8bits-bus-width emmc.

Much regards,

Xavier.

ラベル(2)
0 件の賞賛
返信
7 返答(返信)

1,158件の閲覧回数
xaviercarcelle
Contributor I

Dear Igor,

thanks a lot for your reply. Due to urgent matter with this issue, could it be possible that you could build a uImage based on the 4bits width emmc so I can try it on custom board ?

Much regards,

Xavier.

0 件の賞賛
返信

1,158件の閲覧回数
xaviercarcelle
Contributor I

Dear Igor,

could it be possible to use the archive "IMX6_M6.0.1_2.1.0_MFG_TOOL"

This archive uses in "files", uboot/zImage/dtb that can be recompilable from dts for 4bits emmc ?

Much regards,

Xavier.

0 件の賞賛
返信

1,158件の閲覧回数
xaviercarcelle
Contributor I

Dear Igor,

using "MFGTool (v2.3.2)" + UCL/UTP scripts (available with that tarsal) a kernel is loader in imx6 cram (Linux version 3.0.35-2666-gbdde708), we were unable to write into /dev/mmcblk0 as the emmc on our custom boards is 4bits bus-width. The kernel does not detect the emmc on 4bits as we guess this kernel is configured for 8bits bus-width.

However, after a few seconds, the EMMC appears in the kernel and we detect /dev/mmcblk0 and are able to read it.

Our technical understanding is that the kernel is firstly accessing the emmc in 8bits mode but after some retries, it falls-back in 4bits mode ? Coud it be a good hypothesis ?

Much regards,

Xavier.

0 件の賞賛
返信

1,158件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Xavier

in general yes, kernel can check EXT_CSD[BUS_WIDTH] and

continue with changed bit mode.

Best regards
igor

0 件の賞賛
返信

1,158件の閲覧回数
xaviercarcelle
Contributor I

Hi Igor,

do you know where the code snippet in the kernel for this EXT_CSD configuration usage and timeout for 8bits and 4bits ?

We are trying to rebuild a kernel image based on the sha1 of the kernel we use :

Linux version 3.0.35-2666-gbdde708 (r65388@shlinux3) (gcc version 4.6.2 20110630 (prerelease)

but when rebuilding this kernel with 4bits emmc we have a kernel panic :

"Unable to handle kernel paging request at virtual address e1a01000 / pgd = 80004000"

Do you have some hints to rebuild a fresh kernel from the sha1 gbdde708 ?

Best regards,

Xavier.

0 件の賞賛
返信

1,158件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Xavier

please post this to kernel mail list, as this is generic linux question.

Best regards
igor

0 件の賞賛
返信

1,158件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Xavier

emmc bus width can be changed in *.dts file:

&usdhc.. {
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_usdhc..>;
    bus-width = <8>;..

one can refer to attached Yocto Guide for building

procedures. Please elevate additional requirements

through local fae channel.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信