Hello Longbin
可能之前,我的理解有误,我们讨论,你做一下实验,因为你手头有现成的系统,其实这个问题属于linux系统上的一些技巧,并不是I.MX CPU有关的。其他的linux怎么做的,我们都是可以借鉴的:
1. 关闭psplash.
在u-boot命令,加入psplash=false,启动系统后,这个logo就会不显示。
2. 自动登录,不输入用户名和密码
这个我们还需要看看同行们的做法。网上有一些办法,我贴出来,你试试行不行:
(1)/etc/init/tty1.conf 文件修改
exec /bin/login -f root < /dev/tty1 > /dev/tty1 2>&1
(2)使用其他登录登录程序mingetty
# sudo apt-get install mingetty
# exec /sbin/mingetty --autologin root tty1
(1)和(2)两种方式,应该都行。如果可以,选一个就OK了。
Have a nice day!
B.R,
Weidong
Hi Long bin,
更换启动LOGO,需要这样几个步骤:
1. 需要换掉下面的.h文件
./build-x11/tmp/work/cortexa7hf-neon-poky-linux-gnueabi/psplash/0.1+gitAUTOINC+88343ad23c-r15/git/psplash-poky-img.h
2. 如何把上面的.H文件换成你的,你需要制作一个。
制作方法看这里:
YOCTO开机画面修改_t631791611的博客-CSDN博客_yocto开机启动
然后,就可以了。
Have a nice day!
Weidong
非常感谢你的回复。但是这个方式我试过,并且我再试了一次,没有效果。是不是因为版本不同?我的是4.1.15-2.1.0
root@yada:~# cat /etc/inittab
/etc/inittab: init(8) configuration.
$Id: inittab,v 1.91 2002/01/25 13:35:21 miquels Exp $
The default runlevel.
id:3:initdefault:
Boot-time system configuration/initialization script.
This is run first except when booting in emergency (-b) mode.
si::sysinit:/etc/init.d/rcS
What to do in single-user mode.
~~:S:wait:/sbin/sulogin
/etc/init.d executes the S and K scripts upon change
of runlevel.
#
Runlevel 0 is halt.
Runlevel 1 is single-user.
Runlevels 2-5 are multi-user.
Runlevel 6 is reboot.
l0:0:wait:/etc/init.d/rc 0
l1:1:wait:/etc/init.d/rc 1
l2:2:wait:/etc/init.d/rc 2
l3:3:wait:/etc/init.d/rc 3
l4:4:wait:/etc/init.d/rc 4
l5:5:wait:/etc/init.d/rc 5
l6:6:wait:/etc/init.d/rc 6
Normally not reached, but fallthrough in case of emergency.
z6:6:respawn:/sbin/sulogin
mxc0:12345:respawn:/bin/start_getty 115200 ttymxc0
/sbin/getty invocations for the runlevels.
#
The "id" field MUST be the same as the last
characters of the device (after "tty").
#
Format:
<id>:<runlevels>:<action>:<process>
#
1:12345:respawn:/sbin/getty 38400 tty1
龙斌技术部
广东雅达电子股份有限公司
电力智能测控仪器专家 电力测控领域专业制造商
地址:广东省河源市源城区高埔岗雅达工业园
电话:0762-3493926
邮编:517000
网址:www.yada.com.cn
发件人: weidong.sun
发送时间: 2020-06-10 21:10
收件人: long bin
主题: Re: - Re: 怎么去掉或更改login登陆画面?
NXP Community
Re: 怎么去掉或更改login登陆画面?
reply from Wigros Sun in i.MX Processors - View the full discussion
etc/inittab 文件,你打开看看,用什么方式登录,是可以配置的。
类似这样,就是取消了登录界面:
id:3:initdefault:
【注】如果是 id:5:initdefault:就是图形界面登录。
Weidong
Reply to this message by replying to this email, or go to the message on NXP Community
Start a new discussion in i.MX Processors by email or at NXP Community
Following Re: 怎么去掉或更改login登陆画面? in these streams: Inbox
This email was sent by NXP Community because you are a registered user.
You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences
你好!
我屏蔽掉/etc/inittab内的 #1:12345:respawn:/sbin/getty 38400 tty1 ,结果界面上的
Freescale i.MX Release Distro 4.1.15-2.0.1 yada /dev/tty1 yada longbin: 没有了。现在变成没有任何显示。
真让我头大,请帮帮忙,谢谢。
发件人: weidong.sun
发送时间: 2020-06-11 10:40
收件人: long bin
主题: Re: - Re: 怎么去掉或更改login登陆画面?
NXP Community
Re: 怎么去掉或更改login登陆画面?
reply from Wigros Sun in i.MX Processors - View the full discussion
Hello Long,
实际上,从你贴出来的视频看,登录的速度是挺快的。并不是那么迫切地需要修改。
GUI登录,console登录等方式,是可以修改的,可能你说得对,和版本有关系。
你再试试:
systemctl set-default multi-user.target
这个方式应该行。
Weidong
Reply to this message by replying to this email, or go to the message on NXP Community
Start a new discussion in i.MX Processors by email or at NXP Community
Following Re: 怎么去掉或更改login登陆画面? in these streams: Inbox
This email was sent by NXP Community because you are a registered user.
You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences
你好:
不是这个意思,因为login界面很难看,所以让人不舒服。login界面如下:
方法1:把login界面改成我需要的图片。
方法2:没有login界面显示。这样就直接从psplash任务界面到我的应用程序界面,中间没有经历login界面。
发件人: weidong.sun
发送时间: 2020-06-16 12:09
收件人: long bin
主题: Re: - Re: 怎么去掉或更改login登陆画面?
NXP Community
Re: 怎么去掉或更改login登陆画面?
reply from Wigros Sun in i.MX Processors - View the full discussion
Linux 登录界面,无非就是文本界面和图形界面登录,而你当前情况,是觉得图形登录时间有点长,所以,需要切换到文本模式登录,以节约时间。
是这个意思吧。
Weidong
Reply to this message by replying to this email, or go to the message on NXP Community
Start a new discussion in i.MX Processors by email or at NXP Community
Following Re: 怎么去掉或更改login登陆画面? in these streams: Inbox
This email was sent by NXP Community because you are a registered user.
You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences
wigros sun 你好!
登陆的速度是快,但是因为这个界面的存在造成从开机logo到我应用画面有7,8秒延时,并且这个画面不好看,所以需要改动它。
我试了一下systemctl,我这个版本的linux不认识它。
root@yada:~# systemctl --version
-sh: systemctl: command not found
发件人: weidong.sun
发送时间: 2020-06-11 10:40
收件人: long bin
主题: Re: - Re: 怎么去掉或更改login登陆画面?
NXP Community
Re: 怎么去掉或更改login登陆画面?
reply from Wigros Sun in i.MX Processors - View the full discussion
Hello Long,
实际上,从你贴出来的视频看,登录的速度是挺快的。并不是那么迫切地需要修改。
GUI登录,console登录等方式,是可以修改的,可能你说得对,和版本有关系。
你再试试:
systemctl set-default multi-user.target
这个方式应该行。
Weidong
Reply to this message by replying to this email, or go to the message on NXP Community
Start a new discussion in i.MX Processors by email or at NXP Community
Following Re: 怎么去掉或更改login登陆画面? in these streams: Inbox
This email was sent by NXP Community because you are a registered user.
You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences