Weston clone mode on i.MX8MPlus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Weston clone mode on i.MX8MPlus

Weston clone mode on i.MX8MPlus

This post shows a new feature (weston_clone_mode) that many customers need before in i.MX8MPlus. 

The demo works on Linux BSP L5.10.72_2.2.0 and weston branch weston-imx-9.0.

The detailed introduction, running steps and test result are shown in the attached PPT.

Default Extend Mode Pipeline:

inly_huang_0-1705656318160.png

 

Clone Mode Pipeline:

 

inly_huang_1-1705656360406.png

The DSI buffers which as the clone source in the pipeline can also be changed to HDMI or LVDS buffers.

Running Steps:

  • git apply  clone_difResolution.diff
  • source /opt/fsl-imx-xwayland/5.10-hardknott/environment-setup-cortexa53-crypto-poky-linux
  • meson build/ --prefix=/usr -Ddoc=false -Dbackend-drm-screencast-vaapi=false -Dcolor-management-lcms=false -Dcolor-management-colord=false -Dpipewire=false -Dbackend-x11=false -Dbackend-fbdev=false -Dxwayland=true -Drenderer-g2d=true
  • DESTDIR=./opt/weston ninja -C build/ install
  • tar -cvf weston_usr.tar build/opt/weston/usr/*
  • copy the weston_usr.tar to your evk board
  • systemctl stop Weston
  • tar -xvf weston_usr.tar
  • cp -r  build/opt/weston/* / & sync
  • Adding “clone-mode=1”, “clone-connector-id=41” to your /etc/xdg/weston/weston.ini “core” section like picture (1). You can also add “cloneoutput” section like picture (2)  If you decides to use other modes of your screen.
  • systemctl restart Weston
  • 41 or 45 in the pictures are the connector id of the corresponding screens. You can use modetest –M imx-drm to see the connector id.

 

inly_huang_2-1705656464437.png

 

Test Results:

Three displays:

IMG_9524.jpg

Two Displays:

inly_huang_3-1705656693572.png

 

 Reference Link

 i.MX8MPlus :https://www.nxp.com/design/design-center/development-boards/i-mx-evaluation-and-development-boards/e... 

weston: https://github.com/nxp-imx/weston-imx 

weston doc: https://wayland.pages.freedesktop.org/weston/ 

 

 

HPD update

 

Please update the patch to clone_difResolution_add_HPD.diff which supports HPD feature.

Notion: pleas add force-on=true to the output you use as main screen. For example.

inly_huang_0-1711073512332.png

 

 

 

 

 

 

Attachments
Comments

Dear,

        In the previous version, the hot swap function was not supported. When can the updated version be released? Thank you!

 

        Best Regards!

        Jack

100% helpful (2/2)
Version history
Last update:
‎03-22-2024 03:31 AM
Updated by: