zigbee trust centre link key in app.zpcfg

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

zigbee trust centre link key in app.zpcfg

1,007 Views
layengchan
Contributor I

Hi

I have a few questions on trust centre link key and app.zpcfg. I am using the app.zpcfg of JN-AN-1217,  JN-AN-1218. and JN-AN-1189. The reason for doing so is because I am using the coordinator of JN-AN-1217 and using the dimmablelight of JN-AN-1218 and remote control and occupancy sensor of JN-AN-118

1. Is there a detailed user manual on the different inputs possible in the app.zpcfg file and how to use it? Chap 12 of JN-UG-3113 is not helpful enough.

2. I have doubts on how to use trust centre link key. JN-AN-1217 don't have trust centre in coordinator. JN-AN-1218 has but the device table size is 0. JN-AN-1189 has the below trust centre with table size 37. What is the significance of the table size. There is normally only one link key so I don't understand why table size is 0 or 37. Also how to use it. I try to understand JN-UG-3113 chap 11.7.8 and 11.7.9 . It says they are related. I think chap 11.7.8 is referring to APS Key Table. Please confirm. But when I examine the 3 app.zpcfg, there is no entry in the APS Key Table. Please help me to understand how to use the Trust Centre in the code. It is related to the initial network key in the nodes. Sometimes the initial key in the nodes (eg router or dimmable light) is left blank and sometimes it has Preconfigured Trust Centre Link Key. 

pastedImage_1.png

Looking forward to NXP for clarification. Thank you

Labels (1)
0 Kudos
Reply
1 Reply

760 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

 Is there a detailed user manual on the different inputs possible in the app.zpcfg file and how to use it? Chap 12 of JN-UG-3113 is not helpful enough.  

As you know, the document mentions the ZPS 
Configuration Editor in a lot of steps creates a network the channel, etc. 

2.  The JN-AN-1217 and the JN-AN-1189 have the trust center with table size equal to 37. 

The size of the Trust Centre's device table. In this part, the APS table is not setting in this file. 

For the security and the trust center. You can look at the ZigBee PRO Stack User Guide
1.8 Secure Operating Environment
5.8 Implementing ZigBee Security

Regards,

Mario
 

0 Kudos
Reply