qn908x High frequency clock output in deep sleep

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

qn908x High frequency clock output in deep sleep

1,002 Views
joseraffucci
Contributor IV

Can the high frequency clock be enabled while in DS (0)?  I am seeing the clock get shut down when I go into DS but I am not sure if it's me or the MCU doing it yet.  The documentation isn't clear on what the expected behavior for these pins is.  The bits (PAXX_XTAL_OE) are set in the PIO_WAKEUP_EN1 register which implies that there is a power mode component to the functionality.

Edit:

I have XTAL_PDM_DIS and OSC32M_PDM_DIS set to 0 in PMU_CTRL_2 so the clocks themselves should be running.

0 Kudos
9 Replies

667 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Jose Rafucci,

I test this using the demo_apps power_mode_switch of the SDK 2.2 version. Are you using this example to test it?

0 Kudos

667 Views
joseraffucci
Contributor IV

No, I was using the power_profiling example in wireless_examples/bluetooth.

0 Kudos

666 Views
joseraffucci
Contributor IV

Behavior is the same in the power_mode_switch code.  I see a clock on PA25 when in Active and Sleep modes but nothing in either PD mode.  Are you maybe running this in the debugger? 

Added this after initializing the clocks:

    //Enable pass through XTAL to pin 25
    CLOCK_EnableClkoutSource(kCLOCK_Clkout_XTAL, 1);
    CLOCK_EnableClkoutPin(kCLOCK_Clkout_PA25_XTAL, 1);
    //Leave XTAL on when in PD
    SYSCON->PMU_CTRL2 &= ~SYSCON_PMU_CTRL2_XTAL_PDM_DIS_MASK;

0 Kudos

667 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Jose Raffucci,

Sorry for the late reply. I asked the application team about this and you are right, the only modes where the high frequency clock output is enabled is the RUN and SLEEP mode.  

Best Regards,

Alexis Andalon

0 Kudos

667 Views
joseraffucci
Contributor IV

Thank you for confirming the behavior.

0 Kudos

667 Views
joseraffucci
Contributor IV

While the MCU is in sleep mode the system clock to the CPU is stopped and execution of instructions is suspended until either a reset or an interrupt occurs.

That may be true, but I am not trying to use the MCU.  I am trying to feed out the XTAL signal on PA25.

According to the UM, the XTAL can be left powered on when in DS:

pastedImage_2.png

And the CLK_XTAL_OE is fed from the XTAL and not the system clock:

pastedImage_3.png

So the implication is that this should work.  I'm trying to figure out why.  Does the PMU shut off the GPIO?  Doc says that the PIN_MUX_CTRL is ignored when an OE bit is set.

0 Kudos

667 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Jose Raffucci,

I was testing your problem using the SDK example for power mode switch and I'm not having any issue with seeing the frequency on the pin PA25. 

Could you share how are you configuring the PD mode to try to repeat your issue?

Best Regards,

Alexis Andalon

0 Kudos

667 Views
joseraffucci
Contributor IV

nxf46116 wrote:

 I'm not having any issue with seeing the frequency on the pin PA25.

Are you sure about that? 

Here's what I see:

POR (PowerState 0 - PD0): No Clock

Press PB1(PowerState 1 - PD0): No Clock

Press PB1(PowerState 2 - Active): Clock

Press PB1(PowerState 3 - Sleep): Clock

Press PB1(PowerState 4 - PD1): No Clock

0 Kudos

667 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Jose Raffucci,

While the MCU is in sleep mode the system clock to the CPU is stopped and execution of instructions is suspended until either a reset or an interrupt occurs. So if you're using the high frequency clock to supply the MCU this will stop when you enter the sleep mode.

I hope this answer your question.

Best Regards,

Alexis Andalon

0 Kudos