ZigBee PRO Stack debugging (JN5168)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ZigBee PRO Stack debugging (JN5168)

1,356 Views
davidtolar
Contributor I

Hello.

I hope that someone familiar with NXP ZigBee PRO stack for JN516x can help me, maybe someone from NXP team :smileyhappy:.

I would like to ask for help with debugging ZigBee PRO stack for JN516x.

I'm developing a ZigBee HA device based on JN5168 module.

I have a coordinator running ZigBee network. The netwokr is opened for joining.

On JN5168 module I run JN-AN-1189-ZigBee-HA-Demo DimmableLight application.

The problem is, that DimmableLight app won't join the network.

On 802.15.4 sniffer I see, that the DimmableLight app sends Beacon Request command packet and coordinator responds with Beacon packet. This is ok.

The DimmableLight app discovers the network and function ZPS_eAplZdoJoinNetwork(&(sEZModeData.asSavedNetworks[sEZModeData.u8JoinIndex])); in haEzJoin.c is called with proper network descriptor (extended pan id, channel, ... everything match the network).

But ZPS_eAplZdoJoinNetwork() returns with error code 0xC2 ZPS_NWK_ENUM_INVALID_REQUEST.

No detailed info is provided through callback function registered with ZPS_vExtendedStatusSetCallback().

No packet is send on air by the app.

What i forgot to mention is, that I also enabled debug messages, this is the log:

************************

Stack Event

E_STARTUPZPS_EVENT_NWK_DISCOVERY_COMPLETE......NWK Found, Count = 1 

vEZ_SortAndSaveNetworks

*Saving Open NWK ExPANID = 0x  212effff00b026

vEZ_SortAndSaveNetworks sEZModeData.u8DiscoveredNwkCount = 1

API failed in vEZ_JoinSavedNetwork 194

Exhausted NWK Join

************************

The QUESTION IS:

How can I discover what is wrong if I don't have source code for the ZPS_eAplZdoJoinNetwork() function and the stack itself? Is it possible to get souces of the stack?

Please give me a hint.

Thank you,

David Tolar

University of West Bohemia

Labels (1)
0 Kudos
0 Replies