ZPS_APL_APS_E_ASDU_TOO_LONG 0xA0 ASDU is too large and fragmentation is not supported.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ZPS_APL_APS_E_ASDU_TOO_LONG 0xA0 ASDU is too large and fragmentation is not supported.

1,090 Views
dmsherazi
Contributor IV

Hi 

I am trying to send a unicast by using ZPS_eAplAfUnicastAckDataReq but it fails with status code 0xA0 which is 

 

ZPS_APL_APS_E_ASDU_TOO_LONG 0xA0 A transmit request failed since the ASDU is
too large and fragmentation is not supported.

 

From the Zigbee Stack User Guide 

If the APDU size is larger than the maximum packet size allowed on the network, the
APDU will be broken up into fragments (NPDUs) for transmission, provided that
fragmentation has been enabled by setting the ZigBee network parameter Maximum
Number of Transmitted Simultaneous Fragmented Messages to a non-zero value.

 

I am using the Control Bridge Application Note for JN5189. Can someone please point at where exactly to enable / set the  ZigBee network parameter Maximum Number of Transmitted Simultaneous Fragmented Messages to a non-zero value ?

 

0 Kudos
Reply
6 Replies

1,050 Views
dmsherazi
Contributor IV

@EduardoZamora  Can you please help!

0 Kudos
Reply

1,054 Views
dmsherazi
Contributor IV

@nxp Support

0 Kudos
Reply

1,081 Views
dmsherazi
Contributor IV

found it here https://www.nxp.com/docs/en/user-guide/JN-UG-3113.pdf at page 490.  about sending large data. However on the receiving Node I get ZPS_EVENT_APS_DATA_INDICATION but the size is just one APDU size. How to join the fragments on the reciever node and parse the packet?


B.1.1 Enabling/Disabling Fragmentation

In order to allow fragmented data transfers between two nodes, you must
appropriately configure two ZigBee network parameters:
Note 1: Fragmentation is described further in Appendix

 

dostshah_0-1672309839532.png

 

 

dostshah_1-1672310292941.png

 

 

0 Kudos
Reply

1,031 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @dmsherazi

Please consider that JN-UG-3113 corresponds to JN516x devices; for JN5189 devices, please refer to JN-UG-3130 (this User Guide can be found inside JN5189SDK folder > docs > wireless > Zigbee).

Could you please confirm that you have already read the following sections of JN-UG-3130?

  • 6.5.1.1 Unicast
  • 8.1.2.4 ZPS_eAplAfUnicastAckDataReq
  • Appendix B.1 Fragmented data transfers
  • Appendix B.2.2 Fragmented data transmission to sleeping End Device.

Regards,
Eduardo.

0 Kudos
Reply

1,022 Views
dmsherazi
Contributor IV

hi @EduardoZamora  

Thanks for your response. 

I have gone through them. Both my nodes have non zero  Maximum Number of Transmitted Simultaneous Fragmented   and Maximum Number of Received Simultaneous Fragmented
Messages
.

and the message is sent from the tx node. 

AFAIK the acknowledgemets will be handled by the stack and doesnt need me to write code for it specifically.  I am confused about the process of getting the unicast data on RX node in full 

ZPS_EVENT_APS_DATA_INDICATION gives me the first 100 bytes which is the apduSize. So seems to me that thats the first fragment only. 

0 Kudos
Reply

1,008 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

The processes of fragmentation at the sender and de-fragmentation at the receiver are transparent to the applications at the two ends. zps_eAplAfUnicastAckDataReq() function request end-to-end acknowledgment which, when received, generate zps_EVENT_APS_DATA_ACK event.

Please try the following:

1. Increase APDU size to the maximum payload size required by application.

2. Increase FragmentationMaxNumSimulRx/FragmentationMaxNumSimulTx to the maximum fragmentation block number (integer).

3. APS Max Window Size defines how many fragments are sent before an acknowledgment is expected. Set APS Max Windows Size to 1.

Regards,
Eduardo.

0 Kudos
Reply