Where is the Apache_Prod_BringupPORT.eww workspace located ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is the Apache_Prod_BringupPORT.eww workspace located ?

Jump to solution
1,399 Views
jasonchiang
NXP Employee
NXP Employee


Hello Sir,

       I read AN5179 application note. The topic of this application note is MKW40 PHY Test Using DTM. It described that " Open Apache_Prod_BringupPORT.eww workspace in IAR " in section 3.2.1.

Where is the Apache_Prod_BringupPORT.eww workspace located in the Freescale website for downloading ? Kindly need your comment. Thanks !

0 Kudos
1 Solution
1,026 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
3 Replies
1,027 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
1,024 Views
EarlOrlando
Senior Contributor II

Hello,

Unfortunately, the workspace that you are looking for is not available for download. However, you can use the hci_app project which is available in the Kinetis KW40Z Connectivity Software​. This project is located in the path C:\Freescale\KW40Z_Connectivity_Software_1.0.1\ConnSw\examples\bluetooth\hci_app\frdmkw40z\bare_metal\build\iar\hci_app.eww.

If you have any other doubt please don't hesitate on contact me.

Best regards,

Earl Ramírez.

1,024 Views
jasonchiang
NXP Employee
NXP Employee

Hello Earl Ramírez,

    Does this hci_app project can run PHY Test Using DTM for MKW40 ?

0 Kudos