Hi NXP,
Currently setting ap+station mode on NXP wifi module + rsb3730, the following is my topology:
ap1 (ssid: 1234) -------rsb3730(station + ap (ssid:nxp_ap , ip:192.168.8.1)) --------client
The following issues have been discovered so far:
1. When the station cannot connect to ap1, the client connected to nxp_ap, will ping loss when pinging device (ping 192.168.8.1)
2. When the station cannot connect to ap1,sometimes the ssid of nxp_ap cannot be scanned for a short time, but it will be scanned after about 5 seconds.
Attached is the captured device log.
Thank you~
Austin
Dear Weidong,
Yes, I have successfully set mlan0 and uap0 to ap+station. The problem I am currently encountering is: if mlan0 has been unable to connect to ap1 (ssid: 1234) , then uap0 will sometimes hang directly. If mlan0 has successfully connected to ap1 (ssid: 1234) , then everything is fine.
Attached are the steps we have taken to reproduce the problem so far.
Thank you~
BR,
Austin
Dear @austinlee12345 ,
Attachment is for your reference.
The doc is very similar to your application.
Try it, please!
Thanks!
Regards,
weidong
Dear Weidong,
Yes, I have set ap+sta according to the document you provided. This issue will not happen every time. There is a chance that the SSID of uap0 cannot be scanned or uap0 will stop working.
Thank you~
Regards,
Austin
Dear @austinlee12345 ,
I tested it for several times, It is very strange that I have not reproduced the issue you mentioned above.
-- OTA logs
Could you please provide OTA logs for me when the error occurred ?
Thanks!
Regards,
weidong
Dear Weidong,
The attachment is the log I captured using dmesg in the system.
The problem of uap0 stopping may occur after repeating the steps 20~30 times.
When sets the wrong psk in wpa_supplicant config and let mlan0 cannot asscoiate to the ap, I will wait for about 5~10 minutes to observe the status of uap0.
Thank you~
Regards,
Austin
Dear @austinlee12345
>.When sets the wrong psk in wpa_supplicant config and let mlan0 cannot asscoiate to the ap.
--wrong psk in wpa_supplicant is the only condition to cause the issue, right?
-- If password is correct, no issues, right?
[Additional information I need]
1. systemctl status connman.service
run the command, please! then copy logs to me.
2. If psk is not correct, connection will fail, wpa_supplicant should scan AP continuously, check it, then tell me, please!
Thanks!
Regards,
weidong
Dear Weidong,
>.When sets the wrong psk in wpa_supplicant config and let mlan0 cannot asscoiate to the ap.
--wrong psk in wpa_supplicant is the only condition to cause the issue, right? As long as mlan0 cannot connect to the ap, problems may occur.
-- If password is correct, no issues, right? YES
[Additional information I need]
1. systemctl status connman.service
run the command, please! then copy logs to me. --->The attachment is the captured log
2. If psk is not correct, connection will fail, wpa_supplicant should scan AP continuously, check it, then tell me, please! --->yes,wpa_supplicant should scan AP continuously
Thank you
Regards,
Austin
Dear @austinlee12345 ,
In your system, connmand ( connman.service) is also running:
====================================================
* connman.service - Connection service
Loaded: loaded (/lib/systemd/system/connman.service; enabled; vendor preset: enabled)
Active: active (running) since Thu 2024-04-18 05:33:26 UTC; 24h ago
Main PID: 641 (connmand)
Tasks: 1
Memory: 4.9M
CGroup: /system.slice/connman.service
`-641 /usr/sbin/connmand -n
====================================================
So when connection failed, scan will be continued.
Do you really need to use connmand Daemon process?
Regards,
weidong
Dear Weidong
Do you mean that as long as mlan0 continues to scan, uap0 will have a chance to crash, even if they are different interfaces?
Is this a known issue with nxp wifi driver?
Regards,
Austin
Dear @austinlee12345 ,
Please create the main.conf file in /etc/connman/, if there is no connman directory, create it, please!
[General]
NetworkInterfaceBlacklist=wfd0,uap0,p2p0,muap0,mwfd0,p2p1
Then restart your board. and continue your settings and operations.
Regards,
weidong
Dear Weidong,
We currently use this method for verification, but we find that the problem still occurs.
Are there any other suggested methods?
Thank you~
Regards,
Austin