When rsb3730+nxp wifi is set to ap+station mode, ping loss and the ssid cannot be scanned.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When rsb3730+nxp wifi is set to ap+station mode, ping loss and the ssid cannot be scanned.

2,600 Views
austinlee12345
Contributor I

Hi NXP,

Currently setting ap+station mode on NXP wifi module + rsb3730, the following is my topology:

ap1 (ssid: 1234) -------rsb3730(station + ap (ssid:nxp_ap , ip:192.168.8.1)) --------client


The following issues have been discovered so far:

1. When the station cannot connect to ap1, the client  connected to nxp_ap, will ping loss when pinging device (ping 192.168.8.1)

2. When the station cannot connect to ap1,sometimes the ssid of nxp_ap cannot be scanned for a short time, but it will be scanned after about 5 seconds.

Attached is the captured device log.

 

Thank you~

Austin

0 Kudos
Reply
14 Replies

1,404 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Dear @austinlee12345 ,

 

Let me share a document for you.

The document shows how to setup softAP based on i.MX8MM-EVK + 88W8997, BSP version is 5.4.70 , and I also tested it on bsp version 6.6.3.

 

Thanks!

Regards,

weidong

0 Kudos
Reply

2,544 Views
austinlee12345
Contributor I

Dear Weidong,

Yes, I have successfully set mlan0 and uap0 to ap+station. The problem I am currently encountering is: if mlan0 has been unable to connect to ap1 (ssid: 1234) , then uap0 will sometimes hang directly. If mlan0 has successfully connected to ap1 (ssid: 1234) , then everything is fine.

Attached are the steps we have taken to reproduce the problem so far.

Thank you~

BR,

Austin

0 Kudos
Reply

2,552 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Dear @austinlee12345 ,

 

Attachment is for your reference.

The doc is very similar to your application.

Try it, please!

 

Thanks!

Regards,

weidong

0 Kudos
Reply

2,525 Views
austinlee12345
Contributor I

Dear Weidong,

The same problem happened today. uap0 didn't work at all, but the system worked normally. Attached is the log I captured for your reference.

 

Thank you~

Austin

0 Kudos
Reply

2,520 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Dear @austinlee12345 ,

 

Did you try the steps in my document to test SAT + uap ?

 

Regards,

weidong

0 Kudos
Reply

2,497 Views
austinlee12345
Contributor I

Dear Weidong,

Yes, I have set ap+sta according to the document you provided. This issue will not happen every time. There is a chance that the SSID of uap0 cannot be scanned or uap0 will stop working.

Thank you~

Regards,

Austin

0 Kudos
Reply

2,480 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Dear @austinlee12345 ,

 

I tested it for several times, It is very strange that I have not reproduced the issue you mentioned above.

--  OTA logs

Could you please provide OTA logs for me when the error occurred ?

 

Thanks!

Regards,

weidong

0 Kudos
Reply

2,253 Views
austinlee12345
Contributor I

Dear Weidong,

The attachment is the log I captured using dmesg in the system.


The problem of uap0 stopping may occur after repeating the steps 20~30 times.
When sets the wrong psk in wpa_supplicant config and let mlan0 cannot asscoiate to the ap, I will wait for about 5~10 minutes to observe the status of uap0.

Thank you~

Regards,

Austin

0 Kudos
Reply

2,242 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Dear @austinlee12345 

 

>.When sets the wrong psk in wpa_supplicant config and let mlan0 cannot asscoiate to the ap.

--wrong psk in wpa_supplicant is the only condition to cause the issue, right?

-- If password is correct, no issues, right?

[Additional information I need]

1. systemctl status connman.service

run the command, please! then copy logs to me.

2.  If psk is not correct, connection will fail, wpa_supplicant should scan AP continuously, check it, then tell me, please!

 

Thanks!

Regards,

weidong

 

Tags (1)
0 Kudos
Reply

2,234 Views
austinlee12345
Contributor I

Dear Weidong,

 

>.When sets the wrong psk in wpa_supplicant config and let mlan0 cannot asscoiate to the ap.

--wrong psk in wpa_supplicant is the only condition to cause the issue, right? As long as mlan0 cannot connect to the ap, problems may occur.

-- If password is correct, no issues, right? YES

[Additional information I need]

1. systemctl status connman.service

run the command, please! then copy logs to me. --->The attachment is the captured log

2.  If psk is not correct, connection will fail, wpa_supplicant should scan AP continuously, check it, then tell me, please! --->yes,wpa_supplicant should scan AP continuously

Thank you

Regards,

Austin

0 Kudos
Reply

2,228 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Dear @austinlee12345 ,

 

In your system, connmand ( connman.service) is also running:

====================================================

* connman.service - Connection service
Loaded: loaded (/lib/systemd/system/connman.service; enabled; vendor preset: enabled)
Active: active (running) since Thu 2024-04-18 05:33:26 UTC; 24h ago
Main PID: 641 (connmand)
Tasks: 1
Memory: 4.9M
CGroup: /system.slice/connman.service
`-641 /usr/sbin/connmand -n

====================================================

So when connection failed, scan will be continued.

Do you really need to use connmand Daemon process?

 

Regards,

weidong

 

0 Kudos
Reply

2,115 Views
austinlee12345
Contributor I

Dear Weidong

 

Do you mean that as long as mlan0 continues to scan, uap0 will have a chance to crash, even if they are different interfaces?

Is this a known issue with nxp wifi driver?

Regards,

Austin

0 Kudos
Reply

2,085 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Dear @austinlee12345 ,

 

Please create the main.conf file in /etc/connman/, if there is no connman directory, create it, please!

[General]
NetworkInterfaceBlacklist=wfd0,uap0,p2p0,muap0,mwfd0,p2p1

 

Then restart your board. and continue your settings and operations.

 

Regards,

weidong

0 Kudos
Reply

1,692 Views
austinlee12345
Contributor I

Dear Weidong,

We currently use this method for verification, but we find that the problem still occurs.

Are there any other suggested methods?

Thank you~

Regards,

Austin

0 Kudos
Reply