What are the difference between JN5164,JN5164/001 and JN5164/A01? Are these possible to use the same software?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What are the difference between JN5164,JN5164/001 and JN5164/A01? Are these possible to use the same software?

907件の閲覧回数
shigeoakazawa
Contributor I

What is the difference between JN5164,JN5164/001 and  JN5164/A01?   Are these possible to use the same software?

0 件の賞賛
返信
2 返答(返信)

779件の閲覧回数
EarlOrlando
Senior Contributor II

Hello,

There is no differences in the function and features of the JN5164. The suffix /001 and /A01 are for internal use. It does not affect the function and feature of the product.


Best regards,

Earl Ramírez.

0 件の賞賛
返信

779件の閲覧回数
EarlOrlando
Senior Contributor II

Hello,

Please take a look into the microsite in the link below. I think it could be useful for you.

Support Resources for JN516x MCUs|NXP

Regards,

Earl.

0 件の賞賛
返信