Hi
I have been trying to find out the max voltage ratings of VSEN (Pin 11), ASEN1 and ASEN2 (Pins 11 and 13)
Does anyone know what the max voltage ratings of these pins are?
Solved! Go to Solution.
Hello,
I hope all is great with you. Thank you for using the NXP communities.
Please review the information below:
Please note that the nominal operating range is from 0 V to 1.5 V. However, any level between 1.5 V and VDDP has the same effect (as 1.5 V).
I hope this information helps.
Regards,
David
Hello,
I hope all is great with you. Thank you for using the NXP communities.
Please review the information below:
Please note that the nominal operating range is from 0 V to 1.5 V. However, any level between 1.5 V and VDDP has the same effect (as 1.5 V).
I hope this information helps.
Regards,
David
thank you David
Hello @JbaleAlfa
Hope you are doing well.
Could you please help us with more details about which device you are using?
Regards,
Eduardo.