Unable to program flash on TWR-KW24D512

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unable to program flash on TWR-KW24D512

784 次查看
calvinjohnson-b
NXP Employee
NXP Employee

While trying to flash twrkw24d512_thread_router_eligible_device on  TWR-KW24D512, I'm getting an error complaining "protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set and mass erase is disabled". Not sure what can be done. Please help.twr_kw24_flash_protect.jpg

0 项奖励
回复
1 回复

556 次查看
calvinjohnson-b
NXP Employee
NXP Employee

The issue was with the connector used. Problem resolved after installing driver from P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools...  

USB was used to debug.