Tips: how to decrease front-porch period of polling after ZED wakes up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Tips: how to decrease front-porch period of polling after ZED wakes up

636 Views
patrick_pan
NXP Employee
NXP Employee

It is reported that ZED of JN5169 has long front-porch period (RX is enabled) before polling (TX becomes activated) after ZED wakes up . Please refer to following snapshot in which the front-porch period is selected and highlighted as Orange/Amber.

 Front-Porch Period before Polling.png

Please use following way to decrease this long front-porch period  :

1)  add  #include "mac_pib.h" in AN

2)  add  MAC_vPibSetMinBe(NULL, 1); in initial part of AN

The second parameter of MAC_vPibSetMinBe can be changed to 2,3...etc according to real environment , 

but 1 will make the shortest front-porch period .

Labels (3)
0 Kudos
0 Replies